ANALOG DEVICES DELIVERS INDUSTRY’S FIRST PLL SYNTHESIZER WITH HIGH VOLTAGE CHARGE PUMP

-New ADF4113HV extends charge pump power supply voltage up to 16.5 Volts, compared to most PLL synthesizer ICs which are limited to 5 or 6 Volts. -Extended voltage provides wider tuning range for broadband frequency synthesis.

Norwood, MA (06/04/2007) - Analog Devices, Inc. (NYSE: ADI), a global leader in high-performance semiconductors for signal processing applications, today announced the industry’s first PLL synthesizer with a high-voltage charge pump. The ADF4113HV integer-N frequency synthesizer was specifically designed for use in applications with voltage controlled oscillators (VCOs) that have high tuning voltages, and features a high voltage charge pump (15V). The ADF4113HV is ideally suited for the design of products such as private mobile radios (PMR) and communications test equipment. With the addition of the new charge pump, a high voltage VCO can be controlled directly through a passive loop filter, thereby eliminating the need for active loop filters and as a result, reducing BOM cost as well as noise and current consumption.

The ADF4113HV is fully pin-compatible with the company’s other integer-N PLL synthesizers and complements the ADF4113 in those applications which need a large tuning range but where the cost and component count of an active loop filter are undesirable or impractical. The ADF4113HV is also supported by the Analog Devices’ popular ADIsimPLL™ design and simulation software, which greatly simplifies and streamlines the loop filter design and is available for free download at www.analog.com.

“Analog Devices continues to demonstrate its leadership in RF by adding to its vast product portfolio and delivering devices that set new levels of performance,” said Christian Kermarrec, vice president, RF and wireless systems. “With the addition of the ADF4113HV, designers can get the wide operating voltage range and level of accuracy they need, while also saving them significant time and cost.”

About the ADF4113HV PLL Synthesizer
The ADF4113HV operates in frequencies in the range of 200 MHz to 4 GHz and with a power supply ranging from 2.7 V to 5.5 V. The device consists of a low noise phase frequency detector (PFD), a precision high voltage charge pump, a programmable reference divider, programmable A and B counters, and a dual-modulus prescaler (P/P + 1). A simple 3-wire interface controls all of the on-chip registers. The ADF4113HV also features two selectable charge pump currents and digital lock detectors.

Pricing and Availability
The ADF4113HV is available now and is priced at $2.46 per unit in quantities of 1,000.

About Analog Devices PLL Synthesizers
ADI offers a wide variety of PLL synthesizers for use in applications such as wireless base stations, mobile handsets/PDAs, broadband wireless access, industrial and instrumentation, test equipment, and satellite,. ADI’s ADF4xxx family of both single and dual Fractional-N and Integer-N PLLs feature best-in-class performance, phase noise and integration. In addition to the PLL synthesizer components, ADI offers a number of complementary tools that significantly reduce design cycle time and improve time to market. The company’s ADIsimPLL™ development tool continues to be the industry’s choice for PLL circuit design and evaluation software. The free design tool offers a comprehensive PLL design and simulation package for ADI’s range of PLL frequency synthesizers, enabling rapid prototype development and design optimization. Along with ADIsimPLL, ADI provides a complete range of evaluation boards equipped with user-friendly driver software to quickly and accurately design, optimize and evaluate a new PLL. For a complete list and more information on ADI’s PLL synthesizer products, please visit www.analog.com/pll.

About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

1 ADIsimPLL is a trademark of Analog Devices Inc. All other trademarks included herein are the property of their respective owners.

Editor's Contact Information:

Colleen Cronin
781-937-2622

colleen.cronin@analog.com