Norwood, MA (05/09/2011) - Analog Devices, Inc. (ADI), a global leader in high-performance signal processing and the data converter market share leader*, today introduced a 16-bit D/A converter for wired and wireless communication systems that features the industry’s best combination of package size, speed and low noise. The latest member of ADI’s TxDAC® data converter portfolio, the 16-bit AD9146 D/A converter achieves an industry leading data throughput rate of 1.2 GSPS (gigabits per second) and a low-noise specification of -164 dBm/Hz, in a 7 mm x 7 mm LFCSP package. The AD9146 D/A converter also integrates an 8-bit LVDS (low-voltage differential signaling) interface and low-noise PLL (phase-locked loop) clock multiplier, which allow design engineers to implement up to six transmit channels using half the PCB space previously required.
The AD9146 features 2x and 4x interpolators with fine NCO (numerically-controlled oscillator) modulation that enables baseband signals to be placed anywhere in the D/A converter bandwidth to ease design engineers’ system frequency planning. The low noise figure and an IMD (inter-modulation distortion) of 81 dBc at 100 MHz help this component to achieve a superior ACLR (adjacent-channel leakage ratio) of 82 dBc at 122 MHz IF for W-CDMA single-channel applications.
| Product | Sample Availability | Full Volume Production | Price Each In 1,000 Quantities |
Packaging |
|---|---|---|---|---|
| AD9146 | Now | April 2011 | $29.95 | 7 mm x 7 mm 48-lead LFCSP |
The AD9146 can be designed into circuits for communications applications with ADI’s ADRF6701 750 MHz to 1160 MHz quadrature modulator and ADL5371 500 MHz to 1500 quadrature modulator.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
*Analog Devices, Inc. leads the worldwide data converter market with a 46 percent share, according to industry analyst firm Databeans, Inc. in its market research report titled “2010 Data Converters.” Analog Devices’ 46 percent share is larger than the combined market share of the nearest eight competitors.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe.
Bob Olson
781-937-1666
bob.olson@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved