ANALOG DEVICES DELIVERS RADIO FREQUENCY ICS WITH BREAKTHROUGH INTEGRATION FOR BROADBAND COMMUNICATIONS EQUIPMENT

- Monolithic RF IC products reduce component count by more than 75 percent in point-to-point radios, wireless base stations, cable infrastructure, and communications test equipment.

Norwood, MA (04/06/2010) - Analog Devices, Inc. (NYSE: ADI), a global leader in high performance semiconductors for signal processing applications and leading supplier of RF ICs (radio frequency integrated circuits), announced today two new RF ICs for broadband communications systems that reduce component count by more than 75 percent, without compromising performance. The ADRF6655 active mixer or ADRF6510 dual programmable filter and VGA (variable gain amplifier) integrate multiple functions and discrete devices into a single monolithic chip, reducing component count by a factor of four when compared to traditional discrete RF designs. ADI is the only RF IC supplier to offer devices with this level of integration and with the capability to address multiple broadband communications markets, such as point-to-point microwave radios, wireless base stations, cable infrastructure, defense wideband and software-defined radios, cellular repeaters and relays, and communications test equipment.

“Designers of next-generation radio equipment constantly aim to reduce component count and system cost, without sacrificing performance. ADI’s new ADRF6655 integrated broadband mixer and ADRF6510 dual programmable filter and VGA establish new benchmarks in integration, based on our performance-leading and field-proven PLL/VCO, mixer and amplifier technologies,” said Peter Real, vice president, Linear and RF products, Analog Devices. “Both devices solve complex integration challenges for broadband RF system designers who have previously been constrained by the use of multiple discrete circuits and who can now realize new levels of performance and cost efficiency with these highly integrated and highly flexible monolithic RFICs.”

About the ADRF6655 Active Mixer
Operating within the 100 to 2500 MHz frequency range, the ADRF6655 device is a highly-flexible, single-chip, broadband, active mixer with a fully integrated fractional-N phase locked loop (PLL) synthesizer, voltage controlled oscillator (VCO) and associated low dropout (LDO) regulator circuits. The ADRF6655 active mixer is a highly flexible device that provides exceptional performance for both up- and down-conversion applications. The PLL and VCO provide a fully integrated LO (local oscillator) circuit that can also be brought off-chip for external use. The ADRF6655 active mixer operates on a single +5 V supply and features input linearity IP3 (+29 dBm); input compression P1dB (+14 dBm); conversion gain (6 dB), noise figure (12 dB) as well as LO phase noise of -111 dBc at 100 kHz offset. Full specifications and a complete data sheet can be accessed at www.analog.com/pr/adrf6655.

About the ADRF6510 Dual Programmable Filter and VGA
The ADRF6510 is dual channel fully-differential baseband signal processing solution that integrates a matched pair of fully differential low-noise and low-distortion programmable filters and variable gain amplifiers onto a single chip. The ADRF6510 is the first monolithic IC that replaces complex, bulky discrete fixed function filters, saving considerable board area. The matched filter networks provide exceptional flexibility as the corner frequency is fully adjustable in 1 MHz steps, thereby enabling wideband and narrow band support within a single radio design, a key benefit since the available spectrum and bandwidth varies across markets and regions worldwide.

The ADRF6510 VGA provides an adaptable multi-stage adjustable gain control range of 50 dB, a pre-amp prior to the filters provide a 6 dB step; while the variable gain amplifiers that follow the filter networks provide gain range of -5 dB to +45 dB. This allows the user to select and optimize the gain range for high dynamic range radios and eases the drive requirements into the analog to digital converter.

The ADRF6510 is a unique industry first single chip solution that provides low distortion >60dBc IMD3 ideally suited for high order QAM modulation, quadrature (I-Q) communications systems supporting high bandwidth signals up to 56 MHz. A complete data sheet is available at www.analog.com/pr/adrf6510.

Pricing, Availability and Complementary Products
The ADRF6655 is available now in a 6 mm x 6 mm 40-pin LFCSP package and is priced at $9.98 per unit in 1,000-unit quantities. The ADRF6655 is complemented by ADI’s RF/IF amplifiers such as the ADL5601, ADL5602 and ADL5320. The ADRF6510 is available now in a 5 mm x 5 mm 32-pin LFCSP package and is priced at $8.99 per unit in 1,000-unit quantities. The ADRF6510 is well-suited for use with ADI’s ADL5380, ADL5382 and ADL5387 wideband demodulators.

ADI’s RF IC Portfolio Covers Entire RF Signal Chain
Using a unique combination of design skills, system understanding and process technologies, Analog Devices offers the broadest portfolio of RF ICs covering the entire RF signal chain from industry-leading high-performance RF function blocks to highly integrated WiMAX and short-range, single chip transceiver solutions. The RF function blocks include PLL, integrated PLL/VCO and DDS synthesizers; TruPwr™ RMS power detectors and logarithmic amplifiers; variable gain amplifiers; power amplifiers, low noise amplifiers and other amplifiers; RF mixers and direct conversion modulator and demodulator products. These products are supported by a wide range of free design tools to ease the development of RF systems. For more information, visit http://www.analog.com/rf.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

Subscribe to ADI’s News Feed.

Follow ADI on: http://www.twitter.com/ADI_News.

Editor's Contact Information:

Colleen Cronin
781/937-1622

colleen.cronin@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close