NEW DESIGN TOOLS FROM ANALOG DEVICES REDUCE RISK; EASE RF SYSTEMS DEVELOPMENT
- Free ADIsimRF and ADIsimPLL Version 3.1 accelerate RF systems development.
Norwood, MA (01/26/2009) -
Analog Devices, Inc. (ADI), a global leader in high-performance RF ICs for signal-processing applications, today announced the availability of two downloadable software tools that greatly simplify RF systems design. The ADIsimRF™ design tool easily calculates a variety of parameters within an RF system including cascaded gain, noise figure, power consumption, and more. ADIsimPLL™ Version 3.1 development software, a new generation of ADI’s popular phase-locked loop (PLL) circuit-design and evaluation tool, assists users in evaluating, designing, and troubleshooting RF systems exploiting Analog Devices’ family of PLL synthesizers. Both ADIsimRF and ADIsimPLL Version 3.1 design tools are available from ADI’s web site free of charge.
As the industry’s only supplier of all major RF-to-digital functional building blocks that extend from antenna to processor, Analog Devices supports its broad RF-IC portfolio with a comprehensive suite of design tools. RF systems design is an extremely complex and time-consuming process, and the company’s design tools reduce design risk by making the overall RF-to-digital design practice simpler, faster, more accurate, and more robust.
ADI Adds New Tool to its RF Design-Aid Portfolio -- ADIsimRF
The newest addition to ADI’s portfolio of design tools, ADIsimRF furthers the company’s commitment to provide RF-system designers with innovative tools that improve performance and help ease development for both wireline and wireless communications equipment. The ADIsimRF design tool provides calculations for the most important parameters within the RF signal chain, including cascaded gain, noise figure, IP3, P1dB, and total power consumption. The calculator can be easily switched between transmit mode and receive mode where calculations and data entry are input referred. Designers can vary the number of stages up to a maximum of 15, and additional stages can be inserted at any point in the signal chain. In addition, designers can temporarily disable individual stages, clear their data, or remove them completely. ADIsimRF also contains embedded data from many of ADI’s RF ICs. A designer can easily access this data using pull-down menus, thereby eliminating tedious data entry. The tool also includes device tables to assist in component selection. http://www.analog.com/pr/adisimrf.
ADIsimPLL Version 3.1 Adds Support for Latest Highly-Integrated PLLs and Includes New Simulation Capability for Fractional-N Spurious Estimation
Fully compatible with prior releases, the new ADIsimPLL Version 3.1 design tool eliminates time-consuming iterations from the PLL/synthesizer development process, thus ensuring that products reach the market faster. ADI has optimized its ADF4xxx synthesizers for applications such as wireless base stations, LAN, mobile handsets and PDAs, broadband wireless access, industrial, instrumentation and test equipment, satellite, sonar, and CATV. Analog Devices’ ADIsimPLL Version 3.1 design tool offers support for the company’s latest PLL synthesizers, including the highly-integrated ADF4350, ADF9010, ADF4360-9, and the ADF4157. In addition, the design tool includes a new simulation capability for fractional-N spurious estimation. This feature provides an initial assessment of the amplitude and offset of fractional-N spurs. It also allows the user to adjust parameters that set the spur amplitude in response to various loop filter selections, enabling RF designers to incorporate their measurements to further refine the effects of spurs within their system. ADIsimPLL version 3.1 offers an enhanced library of components, including new VCO libraries and improvements to existing component libraries. It also features new loop filter topologies and improvements to the chip-selection algorithm and the power-up simulation. http://www.analog.com/pr/adisimpll.
ADI’s RF IC Portfolio Covers Entire RF Signal Chain
Using a unique combination of design skills, systems understanding, and process technologies, Analog Devices is the only single-source provider of RF ICs for all major RF-to-digital functional building blocks. Complemented by a full suite of design tools, these RF function blocks include DDS (direct digital synthesizer) devices, PLLs, and TruPwr™ power detectors and logarithmic amplifiers. They also include X-Amp® VGAs (variable gain amplifiers), PAs (power amplifiers), LNAs (low-noise amplifiers) and other RF amplifiers, mixers, and direct-conversion modulator and demodulator products. For more information, visit http://www.analog.com/RF.
About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
Editor's Contact Information:
Colleen Cronin
781/937-1622
colleen.cronin@analog.com