HIGH-PERFORMANCE RF POWER DETECTOR SIMULTANEOUSLY DELIVERS RMS AND ENVELOPE OUTPUTS

ADI's ADL5511 TruPwr™ rms and envelope detector is highly accurate and simplifies envelope extraction of high peak-to-average modulated signals in wireless, instrumentation, military and broadband applications.

Norwood, MA (12/15/2010) - Analog Devices, Inc. (ADI), a world-leader in high-performance semiconductors for signal processing applications and RF ICs (radio frequency integrated circuits), today introduced a new highly integrated, high-performance RF detector for use in wireless, instrumentation, defense, and other broadband applications. ADI’s new ADL5511 TruPwr rms (root mean square) and envelope detector (an electronic circuit that takes a RF signal as input and provides an output that represents the envelope of the signal) offers a high level of integration and functionality by combining two RF functions into one small chip, thereby simplifying designs and reducing BOM (bill of materials) cost. View the data sheet and order samples at www.analog.com/ADL5511.

Improving the PAE (power added efficiency) of high-powered amplifiers continues to be a challenge for wireless and broadband equipment manufacturers. Next-generation WiMAX systems and LTE mobile data and voice systems are adopting OFDM (orthogonal frequency division multiplexed) modulation that supports a large number of subcarriers. The high peak-to-average ratio of these modulated signals causes PAs (power amplifiers) to be backed off from their maximum transmit powers significantly, thereby making the PA less efficient. To improve PA efficiency, an envelope detector has become increasing popular. In drain modulation architectures, an envelope detector modulates the PA power supply from the incoming RF signal, thereby only giving the PA the power needed to properly transmit the RF signal. Traditional architectures leave the PA biased at a much higher power level in order to ensure the PA can properly transmit peak power, but are not capable of reducing PA bias when transmitting lower RF power.

Envelope Output

Operating within the 1 MHz to 4 GHz frequency range, ADI's new ADL5511 TruPwr rms and envelope detector provides a unique approach to improving PAE with a smaller footprint and reduced cost and is a highly accurate, easy-to-use means of extracting the envelope of a modulated signal. The envelope output is presented as a voltage that is proportional to the envelope of the input signal. The rms output is a linear in V/V output voltage that is independent of the peak-to-average ratio of the input signal. The extracted envelope can be used for power amplifier linearization and efficiency enhancements, and the rms output can be used for true power measurement. The ADL5511 offers best-in-class performance including ±0.25 dB rms detection accuracy versus temperature; ±0.25 dB envelope detection accuracy versus temperature and a ± 1 dB dynamic range of 40 dB. The ADL5511 is specified across the industry’s widest temperature range of –40°C to +125°C, making it ideal for high-temperature environments found in remote radio heads and power amplifiers. For complete specifications, please view the data sheet and order samples at www.analog.com/ADL5511.

Availability and Pricing

The ADL5511 is sampling now and is available for $7.33 per unit in 1,000-unit quantities.

RF IC Portfolio Covers Entire RF Signal Chain

Using a unique combination of design skills, system understanding and process technologies, Analog Devices offers the broadest portfolio of RF ICs covering the entire RF signal chain from industry-leading high-performance discrete RF function blocks to highly-integrated multi-functional single-chip RF solutions. ADI’s RF portfolio includes TruPwr™ rms power detectors and logarithmic amplifiers; PLL and DDS synthesizers; RF prescalers; VGAs; ADC drivers, gain blocks, LNAs and other RF amplifiers; RF mixers; direct conversion modulator and demodulator products; integrated transceivers, transmitters and receivers and more. These products are supported by a wide range of free design tools, evaluation boards and other design resources to ease the development of RF systems. For more information, visit: http://www.analog.com/rf.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

Follow ADI on: http://www.twitter.com/ADI_News.

Editor's Contact Information:

Colleen Cronin
(781) 937-1622

Colleen.cronin@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close