METALLURGICAL CROSS SECTIONING OF MICROELECTRONIC PACKAGES FOR OPTICAL INSPECTION AND ELECTRON BEAM ANALYSIS

Robert James Burgoyne
Analog Devices, Inc.

Abstract

Advanced integrated circuit packaging technologies present the analyst with a wide range of packaging materials and geometries. Successful cross sectioning of these devices yields critical construction and/or defect information not obtainable from any other analytical method. This paper will address the practice of producing deformation-free encapsulated cross sections for use in package and process development, failure analysis and materials characterization. Sample preparation sequences for plastic, metal and ceramic packages will be reviewed, along with the results obtained during Scanning Electron Microscope (SEM) and Energy Dispersive Spectroscopy (EDS) analysis of the sections.

METALLOGRAPHIC CROSS SECTIONING of microelectronic packages is a valuable analytical procedure widely used within the semiconductor industry. It is used for a variety of reasons, including package qualification, monitoring of the manufacturing process, incoming quality control and failure analysis. Proper implementation yields results that are unambiguous and can be used as either a sole source of information or to validate data gathered from previously performed, non-destructive analytical procedures. Until recently, cross sectioning of microelectronic components and packages was performed using techniques similar to those used in the metallurgical industry. That is, the sectioned mounts were subjected to successively finer fixed abrasives for the grinding process, and polished to the final finish using an aluminum oxide or similar slurry dispensed onto a low to medium napped cloth. While this method may have been acceptable in the past, subjecting today's state-of-the-art microelectronic packages to this type of sample preparation is ineffective and in some cases results in catastrophic damage. This paper details the practical aspects of producing deformation-free encapsulated cross sections of microelectronic packages using readily available consumable items and semi-automatic sample preparation equipment. The resulting cross sections are suitable for optical inspection, dimensional measurements and a variety of electron beam imaging and analytical techniques.

Figure 1 (see appendix) illustrates a typical flow for conducting metallurgical cross sectioning. Certain steps can often be omitted if the cross section is in support of a routinely performed process monitor where established procedures are to be used for the analysis.

Discussion

Package Characteristics. Before plunging into specimen preparation, it is essential to have a general understanding of the physical properties of all materials used in the construction of the package. Table 1 details the diverse properties of the materials that are found within a typical ceramic sidebraze package.

Table 1

Ceramic Sidebraze Package
Typical Material Package Component Physical Properties
Al/O (Ceramic) Package Body Hard, Brittle
Au/Si Die Attach Soft
Ni/Fe/Co Leads/Lid Tough, Ductile
Au and/or Ni Plating Soft/Ductile
Si IC Chip Brittle
Ag/Cu Lead Braze Soft, Ductile
Pb/Sn Solder Soft
W Coatable Refractory Hard, Tough
Al Bond Wires Soft

As can be seen, the industry standard ceramic sidebraze package shown above contains a significant number of highly dissimilar materials. Further advances in microelectronic packaging technologies has substantially increased the complexity of these packages. Ordinarily, the preparation sequence selected is tailored to the predominant component material or the primary component material(s) to be analyzed. However, the analyst must consider all component materials when selecting or developing a sample preparation sequence for this sample class. Ignoring the unique interfaces that are present in a microelectronic package will likely result in preparation induced artifacts. Microelectronic packages are particularly prone to artifacts such as edge rounding, relief, embedding, smearing and fracturing. (Sample preparation artifacts and recommended corrective actions will be discussed at the end of this paper for easy reference.) Preparation induced artifacts could be misinterpreted as flaws in the manufacturing process.

Supplemental Analysis. Metallurgical cross sectioning is a destructive test. As such, it is important to gather as much information as possible about the device to be sectioned prior to the encapsulation process. Doing this will furnish the analyst with a record to fall back on should questions arise such as whether a defect was pre-existing or induced during the preparation sequence.

Devices submitted for routine process monitors (e.g. measuring die attach thickness, plating thickness, etc.) require little or no preliminary analysis. Nonetheless, since many section requests are in support of a failure analysis where a specific defect is of interest, supplemental analysis is often required.

In order to better understand the package architecture and to successfully section through a specific plane of interest, a number of supplementary analysis techniques should be considered prior to encapsulation. These include, but are not limited to, radiography, ultrasonic imaging, fine and gross leak testing, die penetration and macro photography. A detailed discussion of these techniques is not pertinent to this paper and therefore will not be included.

Figure 2 illustrates the results obtained during radiographic inspection of a plastic multi-chip module that will be sectioned for this paper. Note the double sided circuit board substrate, printed interconnects, thru-holes, and bonding wires.

Figure 2

plastic multi-chip module - Figure 2

Sample Considerations. Cleanliness is one of the most important factors in a cross sectioning environment. A clean, well organized and ergonomic laboratory will not only increase efficiency, but eliminate the potential for cross contamination when dealing with the many different preparation abrasives.

Although a clean working environment is important, package cleanliness is paramount. A properly cleaned package is critical in obtaining a tight bond between the mounting resin and all external package surfaces. Conversely, a package contaminated with identification labels, pencil or felt tip marker residue, finger oils or other hydrocarbons will usually lead to poor adhesion and, ultimately, package to resin delamination.

Cleaning is best accomplished by putting the package in a beaker filled with acetone, and then placing the beaker in an ultrasonic tank that is operated for several minutes. (Of course, the cleaning technique best suited for your application may vary. Some materials may be adversely effected by either acetone or ultrasonic exposure. It is always best to consult with the package vendor or other cognizant source before selecting a cleaning agent.) The high frequency cavitation produced by the sonic cleaner ensures that surface foreign material is removed from tight spaces. All handling of the package from this point forward should be done with a clean pair of stainless steel or plastic tweezers to prevent re-contamination. After removing the package from the beaker, immediately dry it with a blast of N2 gas or microscopically pure air. The use of compressed air from a facilities system is not recommended for sample drying. Hydrocarbons from the compressor oil and/or contamination from piping lines are always present and would be deposited onto the package during such a drying process. Placing the package in a low temperature (~50°C) vacuum bake-out oven for approximately 10 minutes is recommended for extracting any adsorbed residual moisture from the pores of the packaging material.

Encapsulation. The first part of the encapsulation process is to position the package in the sample cup such that the plane of interest will ultimately be parallel to the cutting blade. More often than not, it is necessary to support the package. This is typically accomplished by using plastic "spring" clips, double sided adhesive tape or PSA backed cardboard. If plastic clips are used for support, they must be cleaned in the same manner as with the package.

Microelectronic packages are fragile and cannot withstand the tremendous heat and pressure associated with compression molding. For this reason, cold mounting materials are used for the encapsulation process. Figure 3 provides a simple comparison of the three most commonly used cold mounting materials and their relevant properties.

Figure 3

Comparison of cold mounting materials - Figure 3

For microelectronic applications, epoxies offer the best overall performance. Moderate heat generation during polymerization results in minimum shrinkage, while at the same time providing the high level of hardness necessary for proper edge retention. The only drawback to epoxies is the lengthy cure time; however, this time is generally a small fraction of the overall time required to complete an analysis.

The use of a vacuum impregnation chamber and a pressurization vessel are highly recommended when casting microelectronic packages. Vacuum impregnation is a process in which both the sample cup and resin mixture are placed in a chamber and evacuated using a stand alone vacuum pump. The vacuum removes entrapped air from the pores and other small topographical features of the package, making it possible for the resin to impregnate and consolidate the whole structure. (For best results, cast only enough resin to cover the package, if applicable, and then slowly return the chamber to atmospheric pressure. Although short in duration, the back pressure will further the penetration of resin into the confined areas of the package. Repeat the process and completely fill the sample cup.) Optimum resin penetration is achieved when the sample cup is placed in a pressure vessel and subjected to 40 psi of pressure for a minimum of five minutes.

For most metallurgical applications, satisfactory results can be obtained by using either a vacuum impregnation system or a pressurization system. However, microelectronic packages are one of the few classes of samples that benefit from using both systems. Although the vacuum impregnation system satisfactorily removes entrapped air from the sample, surface tension often prevents the resin from filling extremely small topographical features, such as those on the surface of an integrated circuit. The benefit of the pressurization system is that the pressure helps overcome the surface tension factor and forces the resin into these tight areas.

Figure 4 shows the surface of an integrated circuit after sample preparation. The package was vacuum impregnated using epoxy resin and then placed in a pressure vessel at 40 psi for five minutes. Note that the resin conforms to the topography of the integrated circuit. Furthermore, note the minimal shrinkage observed at the passivation to epoxy interface. The sample was imaged in a SEM in BSE mode (atomic number contrast) at 2,200X magnification.

Figure 4

Integrated Circuit Surface - Figure 4

Sectioning. One might think that the sectioning process is the "easiest" part of the sample preparation sequence; simply place the mount in a holding fixture, attach it to the saw, and begin sectioning. However, proper sectioning is critical in that it establishes the baseline for the rest of the sample preparation process. The sectioning process will always induce some level of deformation; however, with a thorough understanding of the parameters that affect sectioning, initial damage can be minimized and the time spent on subsequent preparation steps will be significantly reduced. Conversely, a haphazard approach to sectioning could create initial deformation that is irreversible.

Table 2 provides a quick reference of the sectioning parameters of concern and the optimum settings for sectioning microelectronic packages.

Table 2

Sectioning Parameter Optimum Selection for Sectioning
Microelectronic Packages
Cutting Blade Low concentration (10LC), 5" Diamond Wafering Blade
Cutting Fluid Water based; good lubrication and cooling properties; constant spray application
Applied Load 150 grams - 200 grams for high speed sectioning
Blade Speed 1,500 rpm -1,800 rpm range provides best results; least deformation
Blade Dressing Continuous dressing; one dress cycle for each sample cut
Sample Fixturing Able to securely hold mount for sectioning

Direction of cut and sample orientation are also key factors when sectioning microelectronic packages. As a general rule, it is best to orient the sample, with respect to blade rotation, such that the brittle material is cut in compression. Doing this will minimize delamination and/or fracturing of the brittle component material. (Experience has shown that it is always best to section microelectronic packages with the silicon chip in compression, even in the case of brittle ceramic substrates. This is critical when packages are sectioned prior to encapsulation; however, it is a good practice to follow this rule even when sectioning encapsulated packages.) Furthermore, the mount should be positioned such that the smallest dimension of the package is parallel to the saw blade. This will result in faster cutting of the sample without a sacrifice in the quality of the section.

Figure 5 illustrates the least and most desirable orientations of the mount with respect to a brittle component and the smallest package dimension.

Figure 5

Mount Orientations - Figure 5

Figure 6 shows an "as cut" ceramic dual-in-line package (lid removed) that was sectioned using the criteria established in Table 2. Note the "crisp" interfaces that exist between the silicon chip, silver filled epoxy die attach and ceramic substrate; the absence of fracturing or cracking of the silicon chip; and the lack of smearing of the soft silver filled epoxy die attach material. This "as cut" sample was imaged in a SEM in secondary electron mode at 50X magnification.

Figure 6

'As Cut' Ceramic Dual-In-Line Package - Figure 6

Tables 3 and 4 (see appendix) detail the preparation sequences for ceramic and metal alloy packages and plastic packages, respectively. These tables should be referenced when reading the following process descriptions.

Planar Grinding. The purpose of the planar grinding, or lapping, process is to: 1) remove the initial deformation induced during sectioning, 2) produce a uniform flatness across all component materials and 3) bring multiple mounts into a common polishing plane.

To begin the overall grinding sequence, sectioned mounts are loaded onto a carousel type sample holder so that several mounts can be prepared simultaneously. Before loading, however, bevel the sectioned end with #240 silicon carbide (SiC) paper, taking care not to grind into the edge of the package. After loading, gently color the sectioned area (that is, the area that will be ground) of each mount with a black indelible felt tipped marker. Doing this will make it easier to identify when all the mounts are at a common polishing plane.

Planar grinding of ceramic and metal alloy microelectronic packages is best accomplished using a 15µm water based, poly-crystalline diamond suspension applied onto a hard lapping plate. Since free abrasives are much less aggressive than fixed abrasives, the material removal rate will be lower. Planar grinding in this fashion usually takes about 10 - 15 minutes, considerably longer than the time required when fixed abrasives are used. This is an acceptable trade-off when considering the benefits of reduced deformation and a decrease in the likelihood of forming cracks. Lapping is also very effective at maintaining the flatness of packages containing highly dissimilar materials. The use of an abrasive greater than 15µm for planar grinding is not recommended. Even when applied onto a hard lapping plate, the larger abrasives cause considerable, and sometimes irreversible, damage to the silicon chip.

Samples containing predominately soft and ductile materials are prone to smearing, distortion and embedding of the rolling abrasives. Samples of this category are frequently planarized using a fixed abrasive technique. This is an acceptable approach when all the component materials are soft. However, if the plane of interest includes the silicon chip, or other brittle component, an advanced technique must be employed to prevent damage to the brittle component material. In this situation, a medium-hard lapping plate, with a 9µm oil based, poly-crystalline diamond suspension is used for planar grinding. Minimizing the abrasive size, plate speed and applied force per sample significantly reduces the likelihood of smearing and embedding, while at the same time maintaining sample flatness and the integrity of the brittle component. This advanced approach will take longer, sometimes up to 30 minutes; nonetheless, the benefits of rolling abrasives on lapping plates make it time well spent.

In both cases described above, the condition of the lapping surface is very important. A concave or convex surface profile will always result in an increase in grinding time. Conditioning (or dressing) plates is very straightforward and should be performed when planarization times begin to exceed normal or "as expected" limits for the given sample.

Planar grinding is a lengthy process. The frequent application of an extender fluid or additional diamond suspension is necessary to prevent "gumming" of the plate surface and to promote material removal. During planar grinding, the abrasives are free to go anywhere, including over the edge of the lapping plate and down the drain. Because of this loss of abrasives, it is best to repeatedly re-charge the lapping plate with diamond suspension instead of an extender fluid.

Sample Integrity. The goal of any sample preparation sequence is to remove all deformation induced from the previously performed preparation step. For metallurgical samples, the process usually involves the use of successively finer abrasives, followed by one or more final polishing steps. Microelectronic packages are more delicate and due to their highly diverse materials will not respond well to this methodology.

Sample integrity is the process in which all deformation incurred during planar grinding is removed, thus revealing, for the first time, the true microstructural characteristics of the materials being prepared. The objective of this intermediate step is to satisfactorily remove all deformation created during planar grinding, while at the same time imparting no further deformation. Further, the sequence selected must be capable of maintaining the flatness obtained during planar grinding.

There are several different ways to approach the sample integrity phase of preparation. This is largely due to the wide variety of consumable items that are available to the analyst. As an example, assume that the sample being prepared is a ceramic sidebraze package. Following planar grinding, the analyst could elect to continue power lapping, in which case a medium-hard lapping surface with a 6µm water based poly-crystalline diamond suspension would be utilized. Another option is to use napless, chemotextile products. These products are excellent for use in the intermediate stages of microelectronic sample preparation because they cut aggressively, yet are capable of maintaining the desired flatness of the sample. In either situation, the analyst may choose to add alkaline colloidal silica along with the diamond suspension, thus adding the element of mechanochemical material removal to the process. The sample integrity phase can sometimes be accomplished in one step; however, two steps are often needed to avoid abrupt transitions in abrasive sizes. All sectioned packages described in this paper were subjected to a two step process. Similarities include the use of chemotextile cloths with colloidal silica applied to support mechanochemical material removal. Differences include the abrasives used (6µm/1µm for predominantly hard packages versus 3µm/1µm for predominately soft packages) and, when working with predominately softer materials, a decrease in applied pressure and wheel speed.

When in doubt, or when developing a new procedure, select consumable items that will, as a minimum, maintain a uniform flatness across the sample. In this way, if the first effort fails to yield adequate results, at least the sample will be in an acceptable condition for a second try without having to repeat the planar grinding process.

Final Polish. Once the intermediate stage of sample preparation is completed, the true microstructure of the sample is clearly visible. However, fine abrasive scratches and/or smearing of soft, ductile components are still apparent and must be removed before the surface is considered free from mechanically induced deformation. The goal of final polishing is to do just that: remove all residual deformation from the sample without inducing any artifacts.

Final polishing utilizes submicron abrasives that remove only the slightest amount of material. As such, this final step cannot correct for gross artifacts (i.e. relief, edge rounding, fracturing, etc.) induced during previously performed preparation steps. Attempts to use final polishing to correct for such preparation errors will do nothing more than waste time and expensive consumable items. For the most part, microelectronic packages fall into one of two main categories: predominately hard materials (e.g. ceramic based and metal alloy based) or predominately soft materials (e.g. plastics). As a general rule, hard materials are polished using hard, napless chemotextile cloths and soft materials are polished using low to medium napped cloths. At times, however, it may be necessary to use two final polishing steps. Take, for example, the complex construction of the ceramic sidebraze package detailed in Table 1. In this situation, the first final polish step would concentrate on the hard brittle components. This can often lead to smearing of the softer component materials. A second step would then be needed to polish the softer materials.

With regards to abrasives, hard materials polish very well with straight colloidal silica suspension. Increasing both the speed of the wheel and the applied pressure helps further mechanochemical material removal. Conversely, softer materials polish well using a homogenous mixture of 50% colloidal silica and 50% deagglomerated alumina (0.05µm). Here, time and pressure must be kept to a minimum to reduce the likelihood of generating edge rounding and microstructural relief artifacts.

Vibratory Polishing. In most cases, sample preparation is concluded after the final polishing stage. However, to achieve the ultimate in polish quality, one additional step, vibratory polishing, is required. Vibratory polishers facilitate single or multiple samples and are the least aggressive with respect to material removal. As such, it is not uncommon for this supplementary step to take up to several hours, or even overnight, to complete. (The length of time is dependent upon the quality of the sample after final polishing and the objective of the section itself.) Because of the time involved, it is best to use a low nap or napless cloth with either straight colloidal silica suspension, submicron alumina or a homogeneous mixture of both. (Cloths with a medium or high nap are not recommended. The selective eroding action inherent with these cloths, coupled with long polishing times, will lead to edge rounding and microstructural relief.) Straight colloidal silica works well on both hard and soft materials and, due to the high pH of the aqueous base, will produce a slight etch artifact on most microelectronic package constituents.

Etching. Etching is a broad topic, one that is subject to manufacturer's specifications; the objective of the cross section; preference of the analyst; the methodology employed; and the complexity of the sample. For the purpose of this paper, one specific technique, plasma field delineation, will be discussed.

Plasma systems have long been used by the semiconductor industry for various wafer fabrication processes. Benchtop versions typically found in failure analysis or reliability laboratories can be used for delineation of microelectronic package cross sections. Their ability to provide uniform anisotropic etching makes them ideal for such tasks.

Several gases are available for use in the selective delineation of the deposited layers found on an integrated circuit. These include, but are not limited to, sulfur-hexafluoride (SF6), trifluoromethane (CHF3) and DE-101, a mixture of He, O2 and carbon-tetrafluoride (CF4).

Figure 7 shows the deposited layers of the integrated circuit following a three minute sulfur-hexafluoride (SF6) plasma etch. Note the clean interfaces between the various deposited layers as well as the trench isolation details. This sample was imaged in a SEM, in secondary electron mode, at 2,500X magnification.

Figure 7

Integrated Circuit following Plasma Etch - Figure 7 Oxygen plasma has recently emerged as a means of cleaning organic residue from microelectronic devices following the assembly process. Oxygen plasma can also be used for etching microelectronic packaging materials containing organic elements.

Figure 8 shows the dramatic results obtained when the plastic multi-chip module sectioned for this paper was subjected to an oxygen plasma field for five minutes. Note the relief etch effects observed within the printed circuit substrate, silver filled epoxy die attach and the bulk plastic of the package. The sample was imaged in a SEM, in secondary electron mode, at 500X magnification and 50° tilt.

Figure 8

Plastic Multi-Chip Module after Oxygen Plasma Field - Figure 8

SEM/EDS Analysis: Reflected light microscopes are the analytical tool most frequently used for the qualitative, and, at times, quantitative, examination of metallurgical cross sections. These instruments do, however, have limitations. The wavelength of the light source defines a useful magnification of about 1,000X, and a single focal plane makes imaging samples with significant topographical details nearly impossible. Superior depth of focus, considerably higher spatial resolution, and elemental identification and mapping capabilities make the scanning electron microscope the ideal complement to the reflected light microscope. This section of the paper will focus on the practical application of the scanning electron microscope to the examination of microelectronic package cross sections.

Specimens subjected to electron beam irradiation undergo several complex interactions with the electrons from the primary beam. This interaction volume yields a variety of emission signals that may be collected and processed by one of several chamber mounted detectors. Figure 9 offers a pictorial representation of a typical interaction volume and emission products that are created when a sample is subjected to primary beam excitation. A brief description of the signals that originate from within the interaction volume follows:

Figure 9

Typical Interaction Volume - Figure 9

Secondary electrons (SE): Low energy electrons emitted from a given atom due to the ionization event that occurs when the primary beam electron collides with that atom. Created throughout the interaction volume as a result of inelastic (electron-electron) collisions, SE's typically have electron energy levels less than 50eV. As such, only those SE's created near the surface escape the sample; the remainder are absorbed by adjacent atoms.

Backscattered electrons (BSE): Electrons that pass close to, or encounter, the nucleus of a specimen atom and are subsequently deflected through large angular trajectories with a minimal loss of electron energy. Created throughout the interaction volume as a result of elastic (electron-nucleus) collisions, BSE's have an energy level that is, on average, about 20% lower than their initial accelerating potential. Because of this negligible loss of energy, BSE's are able to escape to the surface from deep within the interaction volume.

Characteristic x-rays: As the incident beam electron strikes an atom, a weak inner-shell electron is ejected. To maintain atomic stability, a higher energy, outer-shell electron fills the vacancy and simultaneously emits radiation whose value is equal to the difference between the energy levels of the two shells. The portion of energy lost by the decay of electrons as they move from outer to inner shells reflects the unique electron transitions of a given element and, as such, are referred to as a characteristic x-ray.

Continuum x-rays: When an incident beam electron interacts with the nucleus of an atom, it is decelerated and inelastically scattered. The resulting loss of energy can range from 0eV up to the initial accelerating potential of the electron at the emission source. This continuum, or white radiation, constitutes the major part of the x-ray spectrum onto which the characteristic x-rays are superimposed.

The scanning electron microscope is an effective analytical tool that can provide a wealth of useful information. A strong understanding of how a sample will react to electron beam irradiation is the only surefire way to achieve optimal results. Examination of the completed sections is fairly straightforward; however, scanning electron microscopy is subjective in that each analyst has their own way of conducting analyses to achieve the desired results. Nonetheless, the following guidelines and helpful hints should be considered when examining the sections.

Sample preparation: Ensure that the sample is clean and dry prior to insertion in the SEM vacuum chamber. If a conductive coating is not tolerable, apply conductive carbon or silver paint to the bulk of the epoxy and down the side to the metal sample holder. This practice will significantly reduce excess charging of the bulk mounting material. Further, understand that prolonged exposure to high vacuum (typically 10-7 Torr) will result in outgassing and shrinking of the epoxy, thus creating small gaps along the periphery of the package. This could be of concern if the sample is to be re-worked after examination of that specific plane of interest.

Coating: There are four interconnected reasons for coating a sample. In short, these are to: 1) improve the signal, 2) increase the spatial resolution, 3) provide conductivity so that excess surface charging can be shunted to ground potential and 4) minimize thermal damage. Coatings fall into two categories: carbon (C) and precious metals (Au, Au/Pd, Pt, etc.). The decision to apply a coating largely depends on the type of analysis being performed. (Remember that the features within microelectronic packages are huge when compared to the submicron features on the integrated circuit. Imaging is often performed at magnifications less than 20,000X; consequently, a 50Å - 100Å thick layer of conductive coating is imperceptible and recommended when X-ray analysis is not being performed.

SE Imaging: The majority of sample "viewing" will be accomplished using secondary electron imaging. This mode of operation is invaluable when the identification of surface structure is the principal objective for the analysis. When performing SE imaging, it is often best to use lower beam accelerating potentials (<7.5kV) to maximize surface topology resolution. This will not only reduce the amount of local charging on the surface of uncoated samples, but will provide better contrast in the image and photomicrograph due to the decrease in penetration of the incident beam. The application of a precious metal film to semiconductor and insulator materials will further enhance the quality of the image and photomicrograph.

Figures 10A and 10B illustrate the effect that accelerating potential has on image resolution and contrast. Shown is silver filled epoxy die attach that has been etched in oxygen plasma for five minutes. Figure 10A was imaged at 3.0kV accelerating potential, and Figure 10B was imaged at 25.0kV accelerating potential. Note the increase in surface resolution, decrease in edge charging effects and inherently better image detail at 3.0kV. Both images were taken at a magnification of 5,000X and at a 40° tilt angle to improve depth of field.

Figure 10A

Silver Filled Epoxy Die Attach - Figure 10A

Figure 10B

Silver Filled Epoxy Die Attach - Figure 10B

BSE Imaging: BSE imaging provides both atomic number contrast and topographical information about the sample being examined. Because BSE yield is significantly lower than SE yield, higher beam accelerating potentials (>15kV) are often needed to increase signal levels. Although charging is not an issue in BSE imaging, a conductive coating is recommended for the reasons described earlier. Any concerns that the image will be of a single contrast (i.e. that of the coating) are unfounded; the vast majority of BSE's are generated well below the thin conductive coating layer.

The number of BSE's generated in a given area of a sample is directly proportional to the average atomic number of the material in that area. BSE images of non-homogeneous samples will therefore inherently show dramatic contrast variations. For example, in BSE images of gold-silicon (Au-Si) eutectic, the Au phases (Z=79) will appear much brighter than the Si phases (Z=14). This atomic number contrast information can prove invaluable when "mapping" different materials in a sample or conducting EDS analysis.

Figures 11A and 11B illustrate the difference between BSE atomic number contrast (11A) and BSE topography (11B) modes of operation. Shown is the plastic multi-chip module sectioned for this paper. Note the more uniform grey shade and "textured" appearance of Figure 11B, whereas Figure 11A has significant contrast variations but lacks depth. Both images were taken at a magnification of 300X.

Figure 11A

Plastic Multi-Chip Module - Figure 11A

Figure 11B

Plastic Multi-Chip Module - Figure 11B

Figure 12 shows the various layers found within a ceramic sidebraze package. Shown, from top to bottom, is the silicon chip, gold/silicon die attach, nickel and cobalt plating layers, sintered tungsten refractory and the ceramic package. The sample was imaged in a SEM, in BSE mode, at a magnification of 1,250X.

Figure 12

Ceramic Sidebraze Package - Figure 12

Figure 13 shows a plastic leadless chip carrier (PLCC) soldered onto a multi-layer printed circuit board (PCB). This assembly was sectioned in an area that did not include the silicon chip, thus making it an "all soft materials" sample. Shown clearly is the bottom of the plastic package; the solder dipped, copper core package lead; the multi-layer PCB; and the solder joint. (Note that the epoxide fully encapsulated the assembly with no air bubble formation in the restricted area between the lead and package body. This further illustrates the benefits of using both a vacuum impregnation chamber and a pressurization vessel during encapsulation.) The sample was imaged in a SEM, in BSE mode, at a magnification of 250X.

Figure 13

Plastic Leadless Chip Carrier - Figure 13

X-ray Analysis: When elemental identification (EDS) is required to complete an analysis, several factors must be taken into consideration. First is the accelerating potential. A general rule of thumb is to select an accelerating potential that is at least 2.5 times the primary x-ray line (in keV) of the heaviest element being detected. For the vast majority of packages, including the one that will be used as an example, that element is lead (Pb), common to most solders and frit seals. The Pb La line appears at 10.55keV; thus, based on this line, the accelerating potential should be set at approximately 26.5kV. However, lead has numerous emission peaks due to its high atomic weight. The Pb Ma line appears at 2.34keV, thus reducing the recommended accelerating potential substantially. This is beneficial when analyzing samples that are mainly nonconductive. Severe local charging can actually deflect the beam away from the primary area of interest, resulting in erroneous data collection. Lowering the kV setting, without compromising the detectability of all potential elements, is therefore highly desirable. If appropriate, a high accelerating potential can initially be used to identify all potential elements present. The accelerating potential can then be lowered to not only reduce charging, but to improve the spatial resolution of x-ray energies at the lower end of the spectrum.

Figures 14A and 14B represent the spectrum obtained when a ceramic sidebraze package (14A) and plastic multi-chip module (14B) were subjected to a whole package EDS analysis.

Figure 14A

EDS Analysis - Figure 14A

Figure 14B

EDS Analysis - Figure 14B

Conductive coating is another factor that needs to be addressed. It is always best to perform an initial x-ray analysis without a conductive coating. This preliminary analysis provides a true and accurate qualitative assessment of all elements contained within the package. When coating is necessary, select carbon, as it is the preferred conductive coating when performing x-ray analysis. It generates only a single peak (~0.25keV) at the low end of the spectra.

A third issue is the scanning mode of the microscope. Most SEM's have three basic modes of operation. These are: 1) Normal scan: the area being scanned is that which is displayed on the screen; 2) Window or partial field: the area scanned is a variable percentage of the total screen area; and 3) Spot: the X & Y deflection coils are fixed at a controllable DC level, thus creating a moveable, single point electron microprobe. Normal scan is generally used when analyzing whole package sections, whereas window or spot mode is used when specific areas, such as plating layers, intermetallics, etc. need to be analyzed.

X-ray mapping is a versatile mode of x-ray analysis used to detect and display the spatial distribution of one or more specific elements in a non-homogeneous sample when multiple elements are being detected. In this application, a specific element is initially selected for detection and display. When the given element is detected, a bright spot is displayed on the SEM screen at the location that correlates to the detection site. Numerous scans will generate a pattern of light regions representing the relative distribution of the selected element. This procedure can be repeated for several different elements, resulting in a series of x-ray maps showing the distribution of all elements of interest.

Figure 15 illustrates the results of an x-ray map performed on the die attach area of the plastic multi-chip module sectioned for this paper. Shown are: 1) a SE image of the site, 2) a silicon (Si) map, 3) a copper (Cu) map and 4) a nickel (Ni) map.

Figure 15

Plastic Multi-Chip Module after X-Ray Map - Figure 15

Artifacts: Microelectronic packages are no different than any other complex sample prepared using metallographic techniques in that improper preparation can lead to induced artifacts. Table 5 details the artifacts that microelectronic packages are more likely to incur and suggestions on how to correct them. The recommended corrective actions listed below are by no means exhaustive and the analyst may have to resort to a "trial and error" method to determine the appropriate course of action.

Table 5

Preparation Artifact Recommended Corrective Action(s)
Relief Minimize polishing times, use napless cloths, use diamond abrasives
Edge Rounding Minimize polishing times, use napless cloths, use epoxide, reduce applied pressure
Smearing Reduce applied pressure, use colloidal silica, increase lubrication, reduce wheel speed
Cracking & Gaps Clean sample before mounting; minimize abrasive size, reduce applied pressure,
Embedded Abrasives Reduce applied pressure, use high viscosity lubricant, use medium nap cloth for polishing
Scratches Clean work area, clean sample thoroughly after each step, finish each preparation step

Conclusions: Proper implementation and utilization of metallographic sample preparation techniques will provide valuable information about the overall quality of microelectronic package components and the assembly process. The data obtained by metallographic sectioning, and subsequent reflected light and electron beam analysis, can be a critical part of failure analysis activities, process and package qualifications and overall quality control. By always considering the properties of all materials in a microelectronic package throughout the sample preparation sequence, the analyst is able to produce deformation free cross sections that can provide a wealth of information not easily obtained from any other analytical technique.

Acknowledgements

The author would like to take this opportunity to thank James Griffin, Hardie Macauley and Andrew Olney at Analog Devices, Inc. and James Nelson at Buehler, LTD., for their editing services, and Bruce Fried at Analog Devices, Inc., for his ultrasonic imaging and radiography support.

References

  1. B. Bousfield, "Surface Preparation and Microscopy of Materials", John Wiley & Sons, LTD., West Sussex, England, (1992).
  2. "Metallography Principles and Procedures", Leco, Corp. (1992).
  3. "Buehler Dialog, Microstructural Analysis Reference Manual", Buehler, LTD.
  4. "Metalog Guide, Your Guide to the Perfect Materialographic Structure", Struers Corp. (1992).
  5. S.N. Chanat, A.M.H. Trujillo, D.C. Zipperian, Buehler Digest, Vol. 27, No. 1, "Advanced Techniques for High Speed Precision Sectioning", Buehler, LTD, (1993).
  6. B.L. Gabriel, "SEM, A User's Manual for Materials Science", American Society for Metals, (1985).
  7. A.M. Glauert, A.W. Agar, R.H. Anderson, D. Chescoe, "Principles and Practices of Electron Microscope Operation", North-Holland Publishing Company, Amsterdam, (1974).

Appendix

Figure 1 (Typical Sample Preparation Flow Chart)

Typical Sample Preparation Flow Chart - Figure 1

Table 3 (Process Description for Ceramic and Metal Alloy Packages)

  SURFACE LUBRICANT ABRASIVE TIME FORCE SPEED ROTATION
PLANAR GRINDING hard lapping wheel water 15µ M poly diamond (water base) until plane 7 psi/sample 120 rpm contra-directional
1ST SAMPLE INTEGRITY napless chemo-textile cloth colliodal silica 6 µ poly diamond (water base) 5 minutes 6 psi/sample 120 rpm complementary
2ND SAMPLE INTEGRITY napless chemo-textile cloth colloidal silica 1 µ poly diamond (water base) 4 minutes 5 psi/sample 120 rpm complementary
1ST FINAL POLISH napless chemo-textile cloth colloidal silica colloidal silica 8 minutes 7 psi/sample 120 rpm complementary
2ND FINAL POLISH low-medium nap cloth water 50% colloidal
silica/50% alumina
2 minutes 5 psi/sample 90 rpm complementary

Table 4 (Process Description for Plastic Packages)

  SURFACE LUBRICANT ABRASIVE TIME FORCE SPEED ROTATION
PLANAR GRINDING medium-hard lapping wheel lapping oil 9µM poly diamond (oil base) until plane 5 psi/sample 90 rpm contra-directional
1ST SAMPLE INTEGRITY napless chemo-textile cloth lapping oil 3µM poly diamond (oil base) 5 minutes 5 psi/sample 90 rpm contra-directional
2ND SAMPLE INTEGRITY napless chemo-textile cloth lapping oil 1µM poly diamond (oil base) 4 minutes 5 psi/sample 90 rpm complementary
1ST FINAL POLISH napless chemo-textile cloth colloidal silica colloidal silica 5 minutes 5 psi/sample 90 rpm complementary
2ND FINAL POLISH low-medium nap cloth di water 50% colloidal
silica/50% alumina
2 minutes 5 psi/sample 90 rpm complementary

Send Feedback X
content here.
content here.

Send Feedback

Close