ADSP-21XXX APPLICATIONS HANDBOOK FILE AREA

The ADSP-21xxx Applications Handbook File Area contains ADSP-21020 source code, utilities, and test data for various DSP algorithms. These code examples were written using pre-VisualDSPTM tools, and they are optimized for the ADSP-21020 architecture. To port the examples to the more recent SHARC platforms (ADSP-2106x, ADSP-2116x) it is necessary to create a VisualDSP project and make the appropriate changes.

The application areas are divided into the files listed below and zipped using PKZIP version 2.04g. Most files contain REAME or .doc files with information on building and running the code.

DFT.ZIP

The file DFT.ZIP contains the following files which are an example of a Discrete Fourier Transform for use with the ADSP-21020 Development Software. A detailed discussion of these operations can be found in the "ADSP-21020 Development Software Tutorial".

DFT.ASM: ADSP-21020 source for an example 64 point DFT

GENERIC.ACH: Architecture file (system description) for DFT example

MAKEWAVE.C: C source for waveform generation utility

MAKEWAVE.EXE: Waveform generation utility (created TEST64 and SIN64)

PLOTCPLX.M: PC-MATLAB script for plotting DFT results

README.DFT: Read first

SIN64.DAT: Sine (and shifted Cosine) table for DFT example

TEST64.DAT: Input data (all real) for DFT example

back to top
FFTCMPLX.ZIP

The file FFTCMPLX.ZIP contains the following files which are code and utilities for running and testing a radix-2 FFT and a radix-4 FFT on the ADSP-21020. A PC-MATLAB script file PLOTLOG.M is included for ploting and comparison of FFT results.

DEF21020.H: Definitions for bits in the ADSP-21020's system regs

DOIT.BAT: DOS batch file to assemble, link, and start simulator

FFT.ACH: Architecture file for FFT

FFT.DOC: ADSP-21020 FFT user notes

FFTRAD2.ASM: ADSP-21020 assembly code for radix-2 FFT

FFTRAD4.ASM: ADSP-21020 assembly code for radix-4 FFT

INIMAG.DAT: Imaginary input array

INREAL.DAT: Real input array

MAKEWAVE.C: Source for FFT test waveform generation program

MAKEWAVE.EXE: Executable for above

PLOTLOG.M: PC-MATLAB script for plotting FFT results

README.FT2: Read first

README.FT4: Read first

TC2.DAT: Real twiddle factors from TWIDRAD2 program

TC4.DAT: Real twiddle factors from TWIDRAD4 program

TS2.DAT: Imaginary twiddle factors from TWIDRAD2 program

TS4.DAT: Imaginary twiddle factors from TWIDRAD4 program

TWIDRAD2.C: Source for FFT twiddle factor generation program

TWIDRAD2.EXE: Executable for above

TWIDRAD4.C: Source for FFT twiddle factor generation program

TWIDRAD4.EXE: Executable for above

back to top
FFTFIR.ZIP

The file FFTFIR.ZIP contains the following code and utilities for running and testing a fast FIR filter on the ADSP-21020.

COEFF.DAT: Coefficient file

DEF21020.H: Definitions for bits in the ADSP-21020's system regs

EZLAB21K.ACH: 21020 EZ-LAB board architecture file

FCOEF.DAT: Filter coefficients

FFIR.ASM: Demonstrates the use of FFTs to implement fast FIR filters

FFIR.EXE: Fast FIR executable file

FFIR.H: Contains preprocessor variable definitions

FFIRCOEF.C: Converts FIR taps into coefficients for FFIR

FFIRCOEF.EXE: Executable for above

IMPULSE.DAT: Impulse data

IMTRANS.DAT: Imaginary transfer function data generated by ffircoef.c

RETRANS.DAT: Real transfer function data generated by ffircoef.c

TC.DAT: Real twiddle factors from TWIDRAD4 program

TS.DAT: Imaginary twiddle factors from TWIDRAD4 program

TWIDRAD4.C: Source for FFT twiddle factor generation program

TWIDRAD4.EXE: Executable for above

_FFTRAD4.ASM: Assembly code for the radix-4 FFT

back to top
FFTREAL.ZIP
The file FFTREAL.ZIP contains the following code and utilities for running the real FFT programs:
rfft2.asm   a real radix-2 FFT
rfft4.asm   a real radix-4 FFT
irfft2.asm  an inverse real radix-2 program
irfft4.asm  an inverse real radix-4 program

DEF21020.H: Definitions for bits in the ADSP-21020's system regs

DOIT.BAT: DOS batch file to assemble, link, and start simulator

EVREAL.DAT: Real even-indexed time domain input data

FFT.ACH: Architecture file for FFT

FFT.DOC: ADSP-21020 FFT user notes

INIMFFT.DAT: Imaginary frequency domain input data

INREAL.DAT: Real time domain input data

INREFFT.DAT: Real frequency domain input data

IRF2TBL.C: Table generation program for irfft2.asm

IRF2TBL.EXE: Executable for above

IRF4TBL.C: Table generation program for irfft4.asm

IRF4TBL.EXE: Executable for above

IRFFT2.ASM: Inverse real radix-2 FFT routine

IRFFT4.ASM: Inverse real radix-4 FFT routine

MAKESPLT.C: Source for a waveform gen. program that will split the even indexed data into one file and the odd indexed data into another. Used for rfft4.asm.

MAKESPLT.EXE: Executable for above

MAKEWAVE.C: Source for FFT test waveform generation program

MAKEWAVE.EXE: Executable for above

ODREAL.DAT: Real odd-indexed time domain input data

PLOTREAL.M: PC-MATLAB script for plotting FFT results of rfft2.asm

README: Read first

RFFT2.ASM: Real radix-2 FFT

RFFT2TBL.C: Table generation program for rfft2.asm

RFFT2TBL.EXE: Executable for above

RFFT4.ASM: Real radix-4 FFT

RFFT4TBL.C: Table generation program for rfft4.asm

RFFT4TBL.EXE: Executable for above

TC2.DAT: Real twiddle factors for radix 2 routines

TC4.DAT: Real twiddle factors for radix 4 routines

THC.DAT: Half cosine table for conversion stage (FFT)

THS.DAT: Half sine table for conversion stage (FFT)

TNC.DAT: (1/N) cosine table for conversion stage (IFFT)

TNS.DAT: (1/N) sine table for conversion stage (IFFT)

TS2.DAT: Imaginary twiddle factors for radix 2 routines

TS4.DAT: Imaginary twiddle factors for radix 4 routines

back to top
FILTER.ZIP

The file FILTER.ZIP holds all the files required for an ADSP-21020 programming example. A complete description of two such examples is given in a section of the "ADSP-21020 User's Manual" called "Assembly Programmer's Tutorial". Refer to that for details. Both examples ("IIRMEM" and "IIRIRQ") filter data using infinite impulse response (IIR) filters. The examples consist of a main calling program and called subroutines. Technical information on the filters themselves is also presented in the user's manual.

CASCADE.ASM: Cascaded biquad filter subroutine (called by main program)

DEF21020.H: Bit position definitions for ADSP-21020 system registers

FIR.ASM: FIR Subroutine

FIRCOEFS.DAT: Coefficient file

FIRTEST.ASM: Example calling routine

GENERIC.ACH: Example architecture file

IIRCOEFS.DAT: Filter coefficients

IRIRQ.ACH: Architecture description file

IIRIRQ.ASM: Main assembly program

IIRMEM.ASM: Main assembly program

INPUT.DAT: Example port emulation file... the input data

MAKEFILE.FIR: Builds the example

MAKEFILE.IRQ: "Make" file used to create the executable main program

MAKEFILE.MEM: "Make" file used to create the executable main program

OUT300.DAT: Example output port result data

README.FIR: Readme file for the FIR filter routine

README.IRQ: Readme file for the IIRIRQ filter routine

README.MEM: Readme file for the IIRMEM filter routine

back to top
FUNCTION.ZIP

The file FUNCTION.ZIP contains the following code and utilities to perform mathematical funtions (sin,cos,tan,exp,sqrt,divide etc..) on the ADSP-21020.

21K.ACH: Architecture file

ACOMPRES.ASM: A-Law compression routine

AEXPAND.ASM: A-Law expansion routine

ASM_GLOB.H: Assembly library include file

ATAN.ASM: Computes arctangent value of a floating point input

DEF21020.H: Bit definitions

DIVIDE.ASM: Floating point divide routine

DIVSGL.ASM: Divide routine to single precision accuracy

EXP.ASM: Exponential routine

ISQRT.ASM: Inverse square root routine

ISQRTSGL.ASM: Inverse square root to single precison accuracy

LOGS.ASM: Logarithm routine

MAKESIN.BAT: Builds the example code and calls up the simulator

POW.ASM: Computes X raised to the Y power of 2 floating point inputs

POW.H: Include file used by power routine

README: Info file

RECIP.ASM: Reciprocal of its floating point input

SIN.ASM: Sine routine

SINTEST.ASM: Example calling routine

SQRT.ASM: Square root routine

SQRTSGL.ASM: Square root to single precision accuracy

TAN.ASM: Tangent routine

UCOMPRES.ASM: Mu-Law compression routine

UEXPAND.ASM: Mu-Law expansion routine

back to top
GRAPHICS.ZIP

The file GRAPHICS.ZIP contains the following code and utilities to perform graphics funtions on the ADSP-21020.

21K.ACH: Architecture file

ACCREJ.ASM: Graphics trivial line accept/reject

ACCREJ.H: Include file for accrej.asm

BEZIER.ASM: Cubic Bezier polynomial evaluation

BITBLT.ASM: Bit block transfer

BRESEN.ASM: Bresenham line drawing

BSPLINE.ASM: Cubic bspline polynomial evaluation

ILLUM3D.ASM: 3-D graphics illumination

MUL44X41.ASM: Multiply 4x4 by 4x1 matrices

POLYEVAL.ASM: N-order polynomial evaluation of two values

README: Graphics & imaging benchmarks

TBLLKUP.ASM: Table lookup with interpolation

TRANSF.ASM: 3-D graphics translation, rotation and scaling

XPROD.ASM: Vector cross product

back to top
IMAGING.ZIP

The file IMAGING.ZIP contains the following sample imaging applications. Each application is a subroutine call whose arguments and return values are described in detail in the source file FILENAME.asm.

CONV3X3.ASM: 3x3 Convolution on an NxN array

HISTO.ASM: Histogram Evaluation

MED3X3.ASM: Median Filtering (3x3)

back to top
JTAG.ZIP

The file JTAG.ZIP contains the following programs that read spl21k stacked-format output files, and write Motorola Exorciser-format S-records for burning EPROMs for the EPROM-based 21020 JTAG Downloader Board. This board is described in an Analog Devices' DSP Division Application Note entitled "A JTAG Boot Downloader for the ADSP-21020".

B2B.C: Reads bytes created by code2bytes.c

C2B.C: Translates object code structure to EPROM bytes

PUB21K.C: Reads spl21k stacked-format output files

PUB21K.EXE: Executable file

PUB21K.H: Include file for pub21k.c

README: Info file

S2C.C: Reads splitter stacked format file, creates code structure

STOX.C: Converts hexadecimal string to integer

back to top
LMS_RLS.ZIP

The file LMS_RLS.ZIP contains the following code and utilities for running and testing the Least Mean Squares (LMS) algorithm, its modified versions, and the Recursive Least Squares (RLS) algorithm.

DESIRED.DAT: Desired data

ERR.DAT: Data file

ERR1.DAT: Data file

ERR2.DAT: Data file

ERR3.DAT: Data file

ERR4.DAT: Data file

ERR5.DAT: Data file

ERR6.DAT: Data file

ERR7.DAT: Data file

ERR8.DAT: Data file

GENERIC.ACH: Contains architecture description

LATLMS.ASM: Performs the LMS algorithm realized with a lattice FIR filter structure with Joint Process Estimation

LLMS.ASM: Performs the leaky LMS algorithm implemented with a transversal FIR filter structure

LMS.ASM: Performs the LMS algorithm implemented with a transversal FIR filter structure

MACROS.H: Contains different macros, especially the DIVIDE macro used in the RLS and the normalized LMS algorithms

NLMS.ASM: Performs the normalized LMS algorithm implemented with a transversal FIR filter structure

README.LMS: Read first

RLS.ASM: Performs the RLS algorithm implemented with a transversal FIR filter structure

SDLMS.ASM: Performs the sign-data LMS algorithm implemented with a transversal FIR filter structure

SELMS.ASM: Performs the sign-error LMS algorithm implemented with a transversal FIR filter structure

SSLMS.ASM: Performs the sign-sign LMS algorithm implemented with a transversal FIR filter structure

SYLMS.ASM: Performs the LMS algorithm realized with a symmetric transversal FIR filter structure

TESTAFA.ASM: Testing shell for the various adaptive algorithms

back to top
MATRIX.ZIP

The file MATRIX.ZIP contains some example matrix multiply routines which operate on matrices of arbitrary dimension on the ADSP-21020.

GENERIC.ACH: ADSP-21020 generic achitecure decription file

MACROS.H: General purpose macros

MATINV.ASM: Inverts a square matrix

MAT_A.DAT: Example input data file for mxnxnxo.asm and mxnxnx1.asm

MAT_A1.DAT: Example input data file

MAT_B.DAT: Example input data file for mxnxnxo.asm

MAT_BB.DAT: Example input data file for mxnxnx1.asm

MXNXNX0.ASM: Matrix times a matrix source code

MXNXNX1.ASM: Matrix times a vector source code

README.MAT: Info file

back to top
MULTRATE.ZIP

The file MULTRATE.ZIP contains the following code and utilities for running and testing multirate filters using the ADSP-21020.

DEC2STG.EXE: Multirate time-based two-stage decimator

DECIMATE.EXE: Multirate time-based decimator

INTERPOL.EXE: Multirate time-based interpolator

INTSTG.EXE: Multirate time-based 2-stage interpolator

RATIOBUF.EXE: Multirate time-based rational rate changer

RAT_2INT.EXE: Multirate interrupt-based rational rate changer

Note: All of the files in this directory are self-extracting compressed files.

back to top
RAD2FIR.ZIP

The file RAD2FIR.ZIP contains the following code and utilities for running and testing a radix-2 FIR filter on the ADSP-21020.

COEFF.DAT: Coefficient file

DEF21020.H: Definitions for bits in the ADSP-21020's system regs

EZLAB21K.ACH: 21020 EZ-LAB board architecture file

FCOEF.DAT: Filter coefficients

GENERIC.ACH: Architecture file

MKR2COEF.C: Converts direct form FIR coefficients into radix-2 FIR coefficients

MKR2COEF.EXE: Executable for above

R2FIR.ASM: ADSP-21020 radix-2 FIR filter

R2FIREZ.ASM: ADSP-21020 radix-2 FIR filter EZ-LAB example

README: Info file

back to top
Send Feedback X
content here.
content here.

Send Feedback

Close