ANALOG DEVICES’ SIGNAL PROCESSING TECHNOLOGY HELPS CERN’S LARGE HADRON COLLIDER ACHIEVE HIGHEST POSSIBLE SUPERCONDUCTING MAGNET PERFORMANCE

Magnetic field measurement instrument board achieves 100 times greater frequency bandwidth and resolution than previous design, contributing to ultra-high-precision beam-forming in world’s most powerful particle collider.
LHC Tunnel

*CERN technician connects superconducting magnets
in the Large Hadron Collider (LHC) tunnel.

Norwood, MA (10/25/2011) - The European Organization for Nuclear Research (CERN) in Switzerland and the University of Sannio, Benevento, Italy, have collaborated on the design of an advanced instrument for measuring magnetic fields in CERN’s Large Hadron Collider (LHC) superconducting magnets. Called the Fast Digital Integrator (FDI) board, this measurement device uses Analog Devices’ A/D converters, analog multiplexers and DSP components to provide the LHC with the highest possible performance achieved to-date in measuring magnetic fields.

The new FDI board enables 100 times the resolution and frequency bandwidth of the previous generation digital integrator. This significant improvement in dynamic range enables scientists to detect even more minute artifacts that contribute to magnetic field variations, field decay and other time dependent phenomena typical in high-field superconducting accelerator magnets that all negatively affect the quality of particle beams under study. The new FDI boards are used at CERN to measure magnetic flux at 10 revolutions per second through fast-rotating calibrated coils that evaluate the magnetic field produced by the LHC’s 8 Tesla accelerator magnets.

“Prior to the FDI board, the available electronic components were not suitable in terms of accuracy or resolution, which in the case of the Large Hadron Collider easily approaches 10 parts per million,” said Pasquale Arpaia, professor of engineering at the University of Sannio. “We chose to work with Analog Devices because the quality of the company’s products, documentation and support are all very high. This helped make it possible for the FDI to reveal new magnetic investigation regions that we were not able to explore before.”

The LHC is the world’s largest and highest-energy particle accelerator, as well as the biggest machine ever built by humans. Construction started in 2003 and the LHC was operational in 2008. Its mission is to probe some of the most fundamental questions of physics and advance the understanding of the most fundamental laws of nature. Watch videos to learn more about CERN: http://cdsweb.cern.ch/collection/Videos.

Analog Devices Components Deliver Speed, Power and Low-noise Performance

Researchers specified the following ADI components for use on the FDI board:

  • A/D converter (AD7634): this 18-bit analog-to-digital converter delivers superior 101-dB signal-to-noise and distortion ratio (SINAD) at the maximum sampling rate of 670 kS/s (thousand samples per second).
  • Multiplexer (ADG406): this multiplexer features a combination of high switching speed, low power dissipation and low on-resistance. ">Multiplexer (ADG406): this multiplexer features a combination of high switching speed, low power dissipation and low on-resistance.
  • SHARC DSP (ADSP-21262): this 32-bit/40-bit floating-point processor is optimized for high-performance signal processing applications with two computational units, 2-Mbit dual-port on-chip SRAM, multiple internal buses to eliminate I/O bottlenecks, and an innovative digital applications interface.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

* Photo Credit: ©CERN.

To subscribe to ADI's News Feed http://www.analog.com/en/homepage/news.xml

Follow ADI on Twitter at http://www.twitter.com/ADI_News

To subscribe to Analog Dialogue, ADI’s monthly technical journal, visit: http://www.analog.com/subscribe

Editor's Contact Information:

Bob Olson
781-937-1666

bob.olson@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close