BesoVideo Eyes Blackfin® Security Camera Solutions for OEMs

         

BesoVideo Co., Ltd. is casting an eye on success with its Blackfin®-based video surveillance designs for OEMs. The BVIPCAM-500A, based on the Blackfin ADSP-BF561 processor, is the newest and most full-featured in the current lineup of designs from BesoVideo. The BVIPCAM-500A provides the basis for solutions including TCP/IP or wireless surveillance cameras.

Designed to speed time to market for companies producing products for China's growing video security marketplace, the BesoVideo BVIPCAM-500A enables video capture using bandwidth-efficient H.264 encoding at D1 resolution.

The systems experts at this specialist design house picked the Blackfin ADSP-BF561, with dual Blackfin cores, because the required capture and encoding demand high performance; the nature of the market also calls for a very cost-effective price. The BF561, running the uClinux™ embedded operating system, handles the H.264 encoding and TCP/IP network protocol in a single high-performance processor.

"Price/performance is key in the midrange and volume end of the video security market," said Ning Huang, Marketing Manager of BesoVideo in Hefei, China. "Blackfin delivers a combination of DSP and control processing in a single powerful chip. That is the critical aspect that allowed us to meet our performance goals while achieving the price point that our solutions need."

Years of experience with Blackfin gave BesoVideo engineers a great deal of confidence in their choice. What's more, developers were able to streamline their integration efforts by using the H.264 Baseline Profile (BP) encoder that Analog Devices has optimized for Blackfin. BesoVideo also called on the uClinux embedded operating system because of its strong support on the Blackfin family.

"Blackfin delivers a combination of DSP and control processing in a single powerful chip. That is the critical aspect that allowed us to meet our performance goals while achieving the price point that our solutions need."
Ning Huang
Marketing Manager
BesoVideo

With its two high-performance Blackfin processor cores, flexible cache architecture, and enhanced Direct Memory Access (DMA) subsystem, the ADSP-BF561 is geared for complex control and signal processing tasks while maintaining extremely high data throughput. Furthermore, the Dynamic Power Management capabilities of Blackfin significantly lower overall power consumption -- important for BesoVideo's applications that run on battery power such as wireless surveillance and mobile DVRs.

BesoVideo is a member of Analog Devices' Third Party Developers, a network of third party developers for Embedded Processing & DSP.

Visit BesoVideo's web site to learn more.

Read more Customer Case Studies like this...

uClinux is a trademark of Arcturus Networks Inc.

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close