| Chapter: 3 | Page: 356 |
| DOC ID: DOC-930 | |
| Change | |
The pointer name is not correct in the description or the example. In the description, change from: ...the pointer is to an array of at least L_TMPNAM characters... change to: ...the pointer is to an array of at least L_tmpnam characters... In the example, change from: change to: | |
| Chapter: 4 | Page: 172 |
| DOC ID: DOC-918 | |
| Change | |
In the Algorithm section, the formula for the gen_gaussian function contains an error. Change from: Change to: | |
© 1995 - Analog Devices, Inc. All Rights Reserved