| Chapter: 2 | Page: 21 | |||||||||||||||||||||
| DOC ID: DOC-440 | ||||||||||||||||||||||
| Change | ||||||||||||||||||||||
Change the biased versus unbiased rounding example in section 2.3.2.7 to the following:
| ||||||||||||||||||||||
| Chapter: 3 | Page: 13 | |||||||||||||||||||||
| DOC ID: DOC-432 | ||||||||||||||||||||||
| Change | ||||||||||||||||||||||
| In Table 3.5 change the text from: Software Interrupt 2 (corresponding to interrupt vector address 0x001c) To: Software Interrupt 0 | ||||||||||||||||||||||
| Chapter: 5 | Page: 8 | |||||||||||||||||||||
| DOC ID: DOC-433 | ||||||||||||||||||||||
| Change | ||||||||||||||||||||||
| Delete the 1st complete sentence of the 3rd paragraph of section 5.5. Replace it with the following sentence: The maximum frequency of an externally generated clock can be deduced from 1/tSCK, as specified in the data sheet for the processor. | ||||||||||||||||||||||
| Chapter: 15 | Page: 21 | |||||||||||||||||||||
| DOC ID: DOC-442 | ||||||||||||||||||||||
| Change | ||||||||||||||||||||||
| On pages 21, 23, 25, 27, change: "- constant" "- constant + C -1" to (to match the function of the assembler): "-[constant]" "-[constant] + C - 1" | ||||||||||||||||||||||
| Chapter: 15 | Page: 40 | |||||||||||||||||||||
| DOC ID: DOC-444 | ||||||||||||||||||||||
| Change | ||||||||||||||||||||||
| Add the following text: * NONE = | ||||||||||||||||||||||
| Chapter: B | Page: 7 | |||||||||||||||||||||
| DOC ID: DOC-431 | ||||||||||||||||||||||
| Change | ||||||||||||||||||||||
| Change Ay1 to MR1 in the line cited in the description. The 2nd line at the label test_2: should read: AF = - AY1, AY0 = AY1; {quotient is simply AY1} | ||||||||||||||||||||||
© 1995 - Analog Devices, Inc. All Rights Reserved