| Chapter: 1 | Page: 7 |
| DOC ID: DOC-611 | |
| Change | |
| The external port address bus width is 20 bits(A0-A19) | |
| Chapter: 7 | Page: 20 |
| DOC ID: DOC-541 | |
| Change | |
Add the following informational bullet:
Consider a situation where the DSP is doing an external memory read from a FIFO. If an interrupt occurs during a read access to external memory, the read may be aborted. The program control jumps into the interrupt service routine (ISR). In that case, the processor will re-issue the same read after returning from the interrupt. While this is not an issue for static memories, it will cause a loss of synchronization with, for instance, FIFO devices. If operation with a FIFO is required, make sure that the read accesses cannot be interrupted. | |
| Chapter: 7 | Page: 27 |
| DOC ID: DOC-612 | |
| Change | |
In point # 1, it is mentioned as:
Maximum Core Speed puts the peripheral: core clock ratio at HCLK = 1/2 CCLK and puts the core clock at CCLK= 1600 MHz. Change to: CCLK= 160 MHz. | |
| Chapter: 10 | Page: 19 |
| DOC ID: DOC-546 | |
| Change | |
| In the code example, DELETE the following lines (lines 2 and 3 on the page): ar = setbit 4 of ar; io(SYSCR)=ar; | |
| Chapter: 12 | Page: 12 |
| DOC ID: DOC-543 | |
| Change | |
Replace the following paragraph:
If the—No Boot on Software Reset—Run mode (RMODE) bit of the Next System Configuration Register has been set to 0, following a soft reset, program flow jumps to address 0xFF0000 and begins executing the boot ROM code at that location to reboot the DSP. A software reset can also be used to reset the boot mode without doing an actual reboot. If bit 4 of the Next System Configuration Register has been set to 1, following a soft reset, program flow jumps to address 0x000000 and completes reset without rebooting the DSP.With the following paragraph: Following a soft reset, program flow jumps to address 0xFF0000 and begins executing the boot ROM code at that location to reboot the DSP. | |
| Chapter: 12 | Page: 35 |
| DOC ID: DOC-614 | |
| Change | |
| Bit 4 of NXTSCR is the RMODE can be set to 0 or 1. Hence it should NOT be shown as RESERVED. | |
| Chapter: 13 | Page: 3 |
| DOC ID: DOC-613 | |
| Change | |
| For the Peripheral Interrupt Identifier 25, the Interrupt Source and destination is Flag IO Interrupt B | |
| Chapter: 21 | Page: 32 |
| DOC ID: DOC-590 | |
| Change | |
| It would be useful to add diagram with the register bits definition, reset value and the I/O address for the CANRML register. The new figure for the CANRML register would be ideltical to figure 21-20. Each bit would be defined as RMLn. The reset value for this register would be 0x0000 and the I/O address would be 0x10-0x00E. | |
| Chapter: 23 | Page: 2 |
| DOC ID: DOC-567 | |
| Change | |
| Replace figure 23-2 in the ADSP-2199x Mixed Signal DSP Controller Hardware Reference with figure B-2 in ADSP-219x/2191 DSP Hardware Reference manual. | |
| Chapter: n/a | Page: 2 |
| DOC ID: DOC-571 | |
| Change | |
| In the Preface, the European Fax number is incorrect. Use +49-89-76903-157 instead. In the Preface, the IP address of the FTP server is no longer valid. Use ftp://137.71.25.69 instead. | |
| Chapter: N/A | Page: 38 |
| DOC ID: DOC-751 | |
| Change | |
Change the bit descriptions for MCDTXPE(bit 2) and MCDRXPE (bit 3) in the SP_MCMC2 register from: 0 = enabled Change to: 0 = disabled | |
© 1995 - Analog Devices, Inc. All Rights Reserved