| Chapter: 9 | Page: 6 |
| DOC ID: DOC-624 | |
| Change | |
| In Figure 9-1 (SPORT Block Diagram), only one SCLK signal is shown. Actually, each SPORT has two clock signals, a transmit clock signal (TCLK) and a receive clock signal (RCLK). | |
| Chapter: 9 | Page: 13 |
| DOC ID: DOC-535 | |
| Change | |
| In the description of the Serial Word Length Select (SLEN) bit field, SLEN is referred to as "the SLEN bit" a number of times. This reference should change to "the SLEN bits" where it appears on page 9-13 and 9-16. | |
| Chapter: 9 | Page: 18 |
| DOC ID: DOC-515 | |
| Change | |
| The last paragraph on the page needs an additional sentence. Change from: An interrupt is generated when the SPx_RX buffer has been loaded with a received word (the SPx_RX buffer is "not empty"). This interrupt is masked out if SPORT DMA is enabled. Change to: An interrupt is generated when the SPx_RX buffer has been loaded with a received word (the SPx_RX buffer is "not empty"). This interrupt will continue to be generated as long as the SPx_RX buffer is "not empty". This interrupt is masked out if SPORT DMA is enabled. | |
| Chapter: 14 | Page: 47 |
| DOC ID: DOC-499 | |
| Change | |
Because flags only can be edge- or level-sensitive, eliminate the following sentence (last sentence on page):
If the flag pin is configured for edge-sensitivity, the FSSR register also specifies the flag pin's sensitivity for rising edge, falling edge, or both edges. | |
| Chapter: 23 | Page: 72 |
| DOC ID: DOC-659 | |
| Change | |
The description of memory bank width selection is confusing on this page. Delete the sentence:Each of these banks can also be configured to support either 8-bit wide memories or 16-bit wide memories on a bank basis. | |
| Chapter: B | Page: 15 |
| DOC ID: DOC-545 | |
| Change | |
| In Table B-1 (I/O Processor Registers Memory Map), delete the entries for the FSPRC and FSPRS registers. There is only an FSPR register at address 0x06:0x008. Also in Table B-1, delete the entries for the FSBERC and FSBERS registers. There is only an FSBER register at address 0x06:0x00C. | |
| Chapter: B | Page: 45 |
| DOC ID: DOC-548 | |
| Change | |
| The default value of the SPORT status register is mentioned incorrectly as 0x0000. The default value of the SPORT status register is actually 0x0004. | |
| Chapter: B | Page: 103 |
| DOC ID: DOC-657 | |
| Change | |
The description of memory bank width selection is confusing on this page. Delete the sentence:Each of these banks can also be configured to support 8-bit-wide or 16-bit-wide memories on a bank basis. | |
| Chapter: n/a | Page: 6 |
| DOC ID: DOC-570 | |
| Change | |
| In the Preface, the European Fax number is incorrect. Use +49-89-76903-157 instead. In the Preface, the IP address of the FTP server is no longer valid. Use ftp://137.71.25.69 instead. | |
© 1995 - Analog Devices, Inc. All Rights Reserved