DUAL OPERATIONAL AMPLIFIER OFFERS LOW NOISE OVER A WIDE VOLTAGE RANGE UP TO 36 VOLTS

Small footprint enables higher level of integration
AD8599

Norwood, MA (09/19/2006) - About the AD8599
Analog Devices’ AD8599 dual operational amplifier (op amp) is designed for medical, instrumentation, automated test equipment (ATE) and other industrial applications that require low noise without sacrificing precision. The industry’s only dual op amp to specify 1-nV/Hz voltage noise at 1kHz over a wide operating voltage range up to 36 V, the AD8599 lowers voltage noise by 80 percent as compared to standard amplifiers. Available in the same package as many single op amps, the AD8599 allows a much higher level of integration.

The low noise and small footprint make the AD8599 easy to use. It is ideal for closed loop gain, error amplifier configurations and transimpedance applications, such as microphone pre-amps, buffers for precision digital-to-analog converters (DACs) and photodiode amplifiers. The AD8599 comes in an 8 lead SOIC (small outline integrated circuit) package, reducing board space requirements. It also reduces the cost of external components by including a compensation capacitor for unity gain stability.

iPolar Process Improves Gain Stability
The AD8599 is designed using Analog Devices’ proprietary iPolar™ high-voltage process technology, which provides best-in-class precision and gain stability. The device also offers 3.5 pA/√Hz current noise and less than 0.001 percent distortion, both of which are required to maintain the highest levels of precision for audio signal sources, transimpedance (current-to-voltage amplification) and other error feedback amplifier circuits that require high closed-loop gain and stability.

Availability and Pricing
The AD8599, available now in full production quantities, is priced at $4.25 in 1,000-piece quantities. Housed in an 8-lead SOIC package, it is specified over a ±5 V to ±15 V voltage range and the –40 degrees C to +125 degrees C extended industrial temperature range.

About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

iPolar™ is a trademark of Analog Devices, Inc. All other trademarks included herein are the property of their respective owners

Editor's Contact Information:

Charlotte Betterley
781-937-1710
781-937-1078
charlotte.betterley@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close