ANALOG DEVICES INTRODUCES INDUSTRY’S FIRST ISOLATED GATE DRIVERS WITH INTEGRATED ISOLATED POWER
| ADuM5230 and ADuM6132 isolated half-bridge gate drivers reduce system cost and size while increasing quality and reliability for motor drives, power inverters, and plasma displays |
Norwood, MA (03/19/2008) - Analog Devices, Inc., a global leader in high-performance semiconductors for signal-processing applications, is introducing the industry’s first isolated half-bridge gate drivers that incorporate isolated power and isolated gate drivers in one package. Competitive products, such as optocoupler isolated gate drivers, require separate power isolation. Integration eliminates components, reduces system cost and size by as much as 50 percent, and improves system reliability and quality by simplifying designs. Furthermore, the new products will come pre-approved with safety approvals normally required for discrete-based isolated power supplies.
Analog Devices’ engineers integrated an isolated power supply and isolated gate drivers in the same package by using the company’s award-winning iCoupler® technology. This provides isolated high-side and low-side outputs together with ADI’s proprietary isoPower™ integrated, isolated power. isoPower leverages iCoupler technology’s chip-scale micro-transformers along with high-voltage CMOS to create an isolated dc-to-dc converter.
About the ADuM5230 and ADuM6132 Isolated Half-Bridge Gate Drivers
The ADuM5230 and ADuM6132 are designed for implementations that include motor drives, plasma displays, and power inverters found in power supplies and solar power converters. On both devices, the integrated, isolated converter powers both the high-side output as well as any external buffer circuitry, eliminating the cost, space, and design complexity associated with external power supply configurations.
The ADuM5230 and ADuM6132 differ in power capability and high-side/low-side isolation configuration. In the ADuM5230, which supplies 150 mW of power, the high-side and low-side outputs are isolated from each other as well as from the inputs. In the ADuM6132, which supplies 250 mW of power, only the high-side output is isolated from the input.
In contrast to gate drivers employing high-voltage level translation methodologies, the ADuM5230 and ADuM6132 offer the benefit of true galvanic isolation between the inputs and outputs. On both products, the outputs may be operated up to ±700 V (peak) relative to each other. On the ADuM5230, the isolated outputs may be operated up to ±700 V (peak) relative to the inputs, thereby supporting low-side switching to negative voltages.
Availability and Pricing
The ADuM5230 will sample and be available in full production quantities in April 2008. Housed in a wide-body SOIC (small-outline integrated circuit) 16-lead package, the ADuM5230 is priced at $2.25 per unit in 1,000-unit quantities. For more information, visit http://www.analog.com/pr/ADuM5230.
The ADuM6132 is sampling now, and will be available in full production quantities in July 2008. Housed is a wide-body SOIC 16-lead package, the ADuM6132 is priced at $2.12 per unit in 1,000-unit quantities. For more information, visit http://www.analog.com/pr/ADuM6132.
About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
iCoupler is a registered trademark and isoPower is a trademark of Analog Devices, Inc.
Editor's Contact Information:
Linda Kincaid
781-937-1472
linda.kincaid@analog.com