Norwood, MA (06/12/2006) -
About the ADL5385
Analog Devices is expanding its portfolio of radio frequency (RF) integrated circuits (ICs) with a quadrature modulator that operates from 50 MHz to 2200 MHz, making it well-suited for low intermediate frequency (IF) and RF applications such as broadband wireless access systems, microwave radio link transmitters, cable modem termination systems and cellular infrastructure. Requiring only a single-ended, two-times local oscillator (LO) input, the ADL5385 converts complex modulation information from the baseband to the final RF input, over a broad range of LO frequencies.
High Dynamic Range and Suppression Specifications Ease High-Order Modulation Applications
The ADL5385 provides exceptional output dynamic range due to the high output power capability (+10 dBm P1dB), high single-ended output linearity (+24 dBm IP3), and low noise floor (–158 dBm/Hz). The –46 dBm carrier feedthrough and –50 dBc sideband suppression at 140 MHz minimizes the need for calibration and nulling in complex high-order modulation applications such as 16 QAM and greater.
The ADL5385 accepts wideband inputs from dc to 700 MHz that are compatible with the output levels of ADI’s AD977x family of TxDAC+® transmit digital-to-analog converters (DACs). The ADL5385 low LO drive requirement of –7 dBm is also compatible with ADI’s ADL4360 series of integrated phase locked loop (PLL) with VCO products. The 2× LO input frequency of the ADL5385 helps to minimize LO pulling in applications where LO isolation and board density are critical.
Availability and Pricing
The ADL5385 is sampling now, with full-production quantities available in September 2006. It is priced at $4.98 per unit in 1,000-piece quantities and is available in a 4 mm × 4 mm, 24-pin lead frame chip scale package (LFCSP).
Analog Devices Wireless Infrastructure Solutions
ADI delivers hundreds of products for the wireless infrastructure market in 2G/3G/4G cellular, WiMAX, microwave, and satellite for single or multicarrier, direct conversion, or superheterodyne radio designs. Among its extensive offerings are RF and IF building block components, RF subsystems, data converters, clock distribution, thermal and power management, power detection and digital signal processing systems based on the TigerSHARC® processor. For more information, please visit www.analog.com/solutions/wireless.
About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
Charlotte Betterley
781/937-1710
781/937-1710
charlotte.betterley@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved