ANALOG DEVICES INTRODUCES VISUALDSP++ RELEASE 4.5 FOR BLACKFIN, SHARC, AND TIGERSHARC PROCESSORS

Free 90-day test drive available for download.

Norwood, MA (07/05/2006) - Analog Devices, Inc. (NYSE: ADI) today announced the availability of VisualDSP++® Release 4.5, the newest release of its integrated software development and debugging environment (IDDE) for Blackfin®, SHARC®, and TigerSHARC® Processors.

Easy to use and easy to install, VisualDSP++ consists of an integrated development environment, debugger, C/C++ compiler, assembler, linker, and simulator. New features in Release 4.5 include a scriptable flash memory programmer and caching project dependencies to improve build times. Another enhancement is that hardware breakpoints can be easily set and cleared from the main user interface window, which offers new levels of usability when debugging, for example, code executing from flash memory. VisualDSP++ Release 4.5 also supports the new Blackfin Multimedia Starter Kit announced earlier.

A free 90-day test drive download or CD of VisualDSP++ Release 4.5 are available. In addition, the Release 4.5 upgrade is downloadable from the ADI web site and is free of charge to all registered users of VisualDSP++; licensed users of the EZ-KIT Lite® evaluation platform may also update their evaluation version of VisualDSP++ software at no charge. Upgrades are available.

About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

VisualDSP++, Blackfin, SHARC, TigerSHARC, and EZ-KIT Lite are registered trademarks of Analog Devices, Inc. All other trademarks included herein are the property of their respective owners.

Editor's Contact Information:

Cynthia Hoye
408-239-0717

cynthia.hoye@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close