Norwood, MA (01/22/2007) - Analog Devices, Inc. (NYSE: ADI), a global leader in high-performance semiconductors for signal processing applications and market leader in amplifier ICs, today continued its long history of meeting the design needs of instrumentation and industrial equipment customers with the introduction of a zero-drift, digitally-programmable instrumentation amplifier (in-amp). Rated over an extended industrial temperature range, the AD8231 is suited for a variety of sensors, including resistance temperature detectors, thermocouples and automotive pressure sensors, in harsh environments where minute signal variations must be accurately detected in the presence of large common-mode voltages. The AD8231 features 80 percent lower input noise than competing devices while delivering rail-to-rail inputs and outputs at up to 1-MHz bandwidth—five times the throughput of the nearest competing zero-drift in-amp¬. Unlike competing devices, the exceptionally low noise characteristics of the AD8231 allow designers of industrial sensors and controls to maintain dc precision over gain.
“Zero-drift instrumentation amplifiers can have high noise at high gains for a variety of reasons, including the presence of chopping noise,” said Steve Sockolov, product line director, Precision Signal Processing, Analog Devices. “However, the trade-off between offset drift and noise becomes untenable as the gain increases to the level demanded by today’s industrial equipment manufacturers. Analog Devices addressed this challenge using a proprietary auto-zero technique that dramatically lowers the in-amp’s noise profile while eliminating the need for external components, such as switched capacitors.”
Rugged Design Is Ideal for Demanding Industrial Applications
Using a three-operational amplifier (op-amp) instrumentation architecture, the AD8231 enhances reliability by integrating auto-zero amplifiers to maintain a voltage offset of only 50 nV/°C across temperature and over years of operation. The AD8231 also features internal gain-setting resistors, which limit gain coefficient temperature drift to 10 ppm/°C. The device’s LFCSP (lead-frame chip-scale package) material was chosen for its reliability and robustness over temperature, which results in a part that is specified from –40°C to 125°C. The package comes with a center paddle, which keeps the part securely soldered to the printed-circuit board in high-vibration environments.
Software Programmability Makes Gain Adjustment Easy
The AD8231 features software programmable gains of 1, 2, 4, 8, 16, 32, 64, or 128, which are programmed through an easy-to-use three-pin interface. The gain can be set using digital logic, which allows users to repeatedly adjust gain once the in-amp has been designed into the system. A pin-strapping gain setting option is also included. The new device operates on a single supply from 3.3 V to 5 V and has rail-to-rail outputs, making it easy to interface to an analog-to-digital converter (ADC). The AD8231 has high impedance inputs of 10 gigaohms, and unlike competing parts, does not suffer performance degradation when using higher impedance sensors.
Flexibility of Design Yields Cost, Space Savings
The AD8231 includes an additional on-chip op-amp, which further extends performance. The op-amp can be used to create a differential output to drive today’s high performance ADCs, or to add or customize gains. The integrated op-amp also provides a tool for additional error correction, level shifting, or filtering. Using the same low-noise auto-zero techniques as the in-amp, the on-chip op-amp also has rail-to-rail inputs and outputs. The ability of the AD8231 to eliminate noise-prone discrete components, such as switched capacitors, combined with the added on-chip signal conditioning of the integrated op-amp, cuts cost by 60 percent and reduces board space requirements by 50 percent compared to other zero-drift in-amps.
Manufactured using Analog Devices’ highly efficient iCMOS™ (industrial CMOS) process technology, the AD8231 achieves a noise level of 32 nV/rt-Hz, five times lower than competitive zero-drift in-amps. The AD8231 also features 122-dB CMR (common-mode rejection), allowing the in-amp to detect very low-amplitude signals in noisy environments.
Compatible with High-Performance ADCs
Ideally suited for industrial controls and sensors requiring a single 3.3-V to 5-V power supply, ADI’s new single-supply in-amp easily interfaces to ADCs and microcontrollers by using the same power supply as digital components. The AD8231 is designed to work well with Analog Devices’ data converters (including the AD7942, AD7685 and AD7980 PulSAR® ADCs), the ADuC702x family of precision analog microcontrollers and ADI’s ADR121, ADR43x and ADR44x voltage reference.
Pricing and Availability
The AD8231 zero-drift, digitally-programmable, gain in-amp is sampling now in a 16-lead LFCSP package with production quantities available in April 2007. The AD8231 is priced at $1.69 in 1,000-unit quantities.
Analog Devices in Industrial
Analog Devices has a more than 40-year heritage of working in concert with its industrial customers to define, develop and deploy complete signal chain solutions that are optimized for their applications. ADI’s legacy of supporting the sector’s long product life cycles with multi-year manufacturing commitments is augmented by the company’s educated sales force, knowledgeable field applications engineers and advanced design support tools that include evaluation boards and SPICE models.
About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
iCMOS is a trademark and PulSAR is a registered trademark of Analog Devices, Inc.
Linda Kincaid
781/937-1472
781/937-1026
linda.kincaid@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved