ANALOG DEVICES DEBUTS INDUSTRY’S SMALLEST 16-BIT QUAD DIGITAL-TO-ANALOG CONVERTER

Extends nanoDAC family with eight new dual and quad devices that pack uncompromised performance in 30 % the board area of existing solutions.
AD5664R

Norwood, MA (02/27/2006) - Analog Devices, Inc. (NYSE: ADI), the world leader in data converter technology, is addressing the growing requirement for smaller industrial and communications designs by introducing the industry’s first 16-bit quad DAC (digital-to-analog converter) in a compact 3 mm x 3 mm, 10-lead LFCSP (lead frame chip scale package) – a development that will free up to 70% more board space. The new 16-bit quad DAC is one of eight new dual and quad devices announced today that extend ADI’s popular line of nanoDAC® converters in small packages. Unlike existing solutions in other packaging that require an external reference, the new nanoDAC devices lower system cost by integrating an on-chip reference and providing the industry’s smallest footprint.

The flagship product – the AD5664R 16-bit quad DAC – offers very low power consumption (5 mW at 5 V including reference), making it an ideal choice for designers of industrial and communications products such as PLC cards, analog I/O boards and base stations which require high resolution in the minimum board space. It integrates four buffered 16-bit D/A converters in addition to an on-chip 1.25-V, 5-ppm per degree C reference.

“Since introducing the family two years ago with the world’s smallest DAC, the nanoDAC product line has become the solution of choice for engineers designing for small form factors,” said Mike Britchfield, product line director, Precision Signal Processing group, Analog Devices. “With the introduction of the AD5664R, Analog Devices has introduced a 16-bit, fully integrated quad converter that lowers system cost and further extends our nanoDAC product family to provide a wide range of offerings that are optimized for space- and cost sensitive industrial and communications applications.”

Expanding the nanoDAC family
In addition to the AD5664R, Analog Devices today is introducing seven nanoDAC converters that offer pin compatible 12-bit to 16-bit resolution in dual and quad configurations with and without on-chip references: the quad AD5624, AD5624R, AD5644R and AD5664, and the dual AD5643R, AD5663 and AD5663R. These new devices add to ADI’s nanoDAC portfolio of smallest package devices, which also features the world’s smallest DAC in SC70 package.

All devices incorporate a power-on reset and a per-channel power-down mode that, in the quad-channel devices, reduces the current consumption of the device to 480 nA at 5 V. In addition, the dual channel devices offer hardware LDAC and CLR functionality and the on-chip precision output amplifier allows rail-to-rail output swing to be achieved, maximizing dynamic range and enabling the device to deliver the performance needed in control and level-setting applications.

Pricing and Availability
The AD5664R, along with the other quad and dual nanoDAC devices announced today, are currently sampling and will be available in full production volumes in April 2006. In addition to the 10-lead LFCSP, all devices are available in 10-lead MSOP (mini-small-outline package). Per-unit pricing ranges from $5.49 to $11.40 for the quad devices and from $5.05 to $6.90 for the dual devices—based on resolution and the inclusion of the on-chip reference—in 1,000-piece quantities.

ADI’s Data Conversion Technology: Critical Bridge Between Analog and Digital
Analog Devices is the world leader in data conversion technology. ADI’s longstanding leadership in data conversion technology stems from an engineering culture that emphasizes deep understanding of the customer’s system challenge, aggressive research and development investing and unmatched mixed-signal design expertise. From application-specific solutions designed to lower system cost to the broadest selection of speed, accuracy size and power consumption in DACs and ADCs, Analog Devices provides the products, technology and support customers need to successfully bridge between real-world analog signals and the digital world of electronic equipment. ADI’s data converters are used widely in consumer electronics, broadband and wireless communications, automotive systems, industrial equipment and medical electronics, as well as a host of other emerging market applications.

About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

nanoDAC is a registered trademark of Analog Devices.

Editor's Contact Information:

Krys Monaco
781/937-1945
781/937-1026
krys.monaco@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close