Norwood, MA (02/06/2008) - Analog Devices, Inc. (NYSE: ADI), a global leader in high-performance semiconductors for signal processing applications and market leader in amplifier ICs, today introduced a digitally programmable VGA (variable gain amplifier) with transmit driver that sets a new standard of performance for driving signals over power lines, cables, and other applications with low impedance. The AD8260 operates on a single 3.3-V power supply and has a transmit driver that produces ±200-mA output up to 100 kHz, and greater than ±100-mA above that frequency. This is an improvement over competing solutions using a discrete VGA, output driver and pre-amp, which consume 90 percent more board space, and require multiple power supplies.
The AD8260 VGA operates at -3dB bandwidth of 200-MHz and includes a 30-dB gain range digitally adjustable in 3-dB gain steps providing the headroom needed for losses introduced in various cabling systems. The new VGA features 2.4nV/rtHz input voltage noise and driver with a built-in gain of 1.5, which is ideal for converting DAC (digital-to-analog converter) differential output signals to a voltage that can directly drive very low impedances. The AD8260 can fully drive a 10 load with 2 Vpp at 10 MHz. In addition, the chip dissipates just 93 mW of power, which is less than half that of competing devices.
More About the AD8260
The AD8260 includes a high-current driver, usable as a transmitter, and a low-noise digitally programmable VGA, which is useable as a receiver, combined in a 5 mm x 5 mm chip-scale package. The receiver section consists of a single-ended input preamplifier and linear-in-dB, differential-output VGA. The differential output facilitates the interface to modern low-voltage, high-speed ADCs (analog-to-digital converters). Versatile single- and dual-supply operation allow gain control of negative-going pulses, such as generated by photodiodes or photo-multiplier tubes, and allows for the processing of band-pass signals on a single supply. The AD8260 preamplifier is user-configurable with external resistors for gains greater than 6 dB.
The driver is set-up to be driven by modern current output DACs, like the high-speed AD9742 12 bit, 3.3 V supply DAC.
Pricing and Availability
The AD8260 is sampling now, with full volume production scheduled for March 2008. The AD8260 is available in a 32-Lead LFCSP (lead-frame chip-scale package) over the extended industrial temperature range -40C to 105C and is priced at $3.79 in 1,000-unit quantities. For more information, visit http://www.analog.com/pr/AD8260.
About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
Linda Kincaid
781-937-1472
linda.kincaid@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved