Norwood, MA (12/19/2006) -
Analog Devices, Inc. (NYSE: ADI) is continuing to expand its broad line of HDMI™ interface ICs with the availability of HDMI v1.3-compatible multiplexer, receiver and transmitter circuits that are helping the high-definition (HD) video market achieve new levels of picture quality and power efficiency. The industry’s broadest portfolio of HDMI (High-Definition Multimedia Interface™) components now includes devices that address the increasing consumer demand for HD content in multimedia products ranging from 1080p “deep color” HDTVs to low-power portable applications, including digital video & still cameras, portable media players and cell phones. Announced today, the multiplexers, receiver and transmitters support the updated HDMI v1.3 standard, which defines the delivery of uncompressed HD content using a single cable to transmit super-high-quality video and audio. Included in today’s announcement are devices for the industry’s key advanced television and video applications:
“The breadth of Analog Devices’ HDMI product suite underscores the role that ADI’s analog and mixed-signal processing expertise is playing in creating an HDTV viewing experience that faithfully converts, conditions and regulates the signals that result in superior, cinema-grade sound and images,” said John Hussey, vice president of High-Speed Signal Processing, Analog Devices. “ADI’s ability to support HD transmission and reception across multiple end products further emphasizes the system-level understanding that has enabled the company to develop HD solutions for the world’s most recognized consumer electronics brands.”
Deep Color Enhances HDTV Image Quality
The AD8196 and AD8197 are the world’s first buffered multiplexers to support the incorporation of HDMI v1.3 2.25 Gb/s “deep color” inputs into HDTV designs and increase the resolution of colors that can be displayed on-screen to 12 bits. The AD8196 and AD8197 also provide 12-dB equalization of TMDS (transition minimized differential signaling) signals over HDMI cable lengths more than 20 meters. The new devices additionally feature on-chip auxiliary multiplexers, which enable display data-channel signal switching, and include integrated TMDS buffers and 50-ohm termination, which combine to reduce parts counts and board space and improve overall signal integrity.
New HDMI v1.3 Receiver Accepts HD and Legacy Analog Inputs
The AD9388A receiver extends ADI’s support for the HDMI v1.3 standard by integrating a 12-channel analog input component digitizer with a dual-port HDMI v1.3 receiver to support multiple analog inputs and HD signals up to 1080p and UXGA resolutions (1600 x 1200 at 60 Hz). In addition to the on-chip adaptive cable equalization feature, the AD9388A integrates 10-bit ADCs to digitize RGB and HDTV sources at up to 170-MHz with 8-bit or 10-bit output formats. The device also embeds HDCP (high-bandwidth digital content protection) key storage and an EDID (extended display identification data) RAM to reduce overall system complexity and cost relative to discrete solutions. Versions of the receiver without internal keys are available for customers who prefer to use their own external EEPROM.
Low-Power Transmitters Bring HDMI v1.3 Support to Handheld Video Devices
The AD9387 is the first low-power transmitter for video-enabled portable consumer electronics that meets HDMI v1.3 specifications. Optimized for high-quality video formats from 720p to 1080i, the transmitter supports both S/PDIF (Sony/Philips digital interface) and 8-channel I2S (inter-IC sound) audio recording formats and transmits either stereo or 7.1-channel surround audio at 192 kHz. This enables digital video cameras, cell phones and other handheld electronics to carry stereo LPCM (linear pulse-code modulation) audio or compressed audio, including Dolby® Digital, DTS® and THX®. The AD9387 consumes just 100 mW of power at 80-MHz and 20 µW during power down, a 55 percent to 90 percent reduction as compared to other transmitters. A version of the new transmitter, the AD9387NK, further reduces cost and system design complexity by allowing for external implementation of HDCP keys.
Availability and Pricing
| Product | Sample Availability | Production Availability | Packaging (Pb-free) | Price (1000 qty.) |
| AD8196 Multiplexer | Now | January 2007 | 56-lead LFCSP | $2.75 |
| AD8197 Multiplexer | Now | January 2007 | 100-lead LQFP | $4.95 |
| AD9388A Receiver | Now | April 2007 | 144-lead LQFP | $9.96 |
| AD9387 Transmitter (80 MHz) | January 2007 | March 2007 | 64-pin LFCSP 76-pin BGA | $4.86 |
| AD9387NK Transmitter (80 MHz) | Now | February 2007 | 64-pin LFCSP 76-pin BGA | $4.39 |
Analog is Everywhere in Advanced TV
As more and more consumers discover the benefits of owning high-definition TVs and home theater systems, equipment manufacturers must continue to raise the performance of video, audio, and display interfaces. Consumers want “cinema-quality” images and audio from their large-screen HDTVs; they want connectivity to the Internet and to their cable set-top boxes, home audio systems and DVD players; and they want it all in systems that are easy-to-use and affordably priced. Analog Devices is committed to supplying the high-performance Advanced TV interface ICs, including video encoders and decoders, analog and HDMI interfaces and audio processors and amplifiers, to enable the ultimate multimedia entertainment experience at home. For more information, visit: www.analog.com/pr/advancedtv.
About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
HDMI and High-Definition Multimedia Interface are trademarks of HDMI Licensing, LLC in the United States and other countries. All other trademarks are property of their respective owners.
Charlotte Betterley
781-937-1710
781-937-1078
charlotte.betterley@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved