POWER SUPPLY SEQUENCER BRINGS BEST-IN-CLASS ACCURACY TO TELECOMMUNICATIONS INFRASTRUCTURE EQUIPMENT

- Highly accurate, flexible ADM1185 quad voltage monitor and sequencer performs power supply sequencing, supervisory and diagnostic functions in wireless infrastructure applications.
ADM1185

Norwood, MA (08/25/2006) - About the ADM1185 Quad Voltage Monitor and Sequencer
Analog Devices today expanded its family of power supply sequencer and supervisory products with a flexible, accurate device that protects against brown out conditions in communications infrastructure equipment. The ADM1185 quad voltage monitor and sequencer is designed for systems with multiple power supplies, like wireless base stations, that require sequencer products to ensure voltage rails are powered up in a controlled manner in order to prevent equipment damage. By providing both a voltage monitoring and sequencing function for up to four power supply rails, the ADM1185 actively controls the order in which the rails are powered up and monitors the system to ensure the rails are quickly powered down if a failure occurs.

High Accuracy and User Programmability
The ADM1185 also features industry-leading precision threshold detection of 0.6V ± 0.8 percent, two times more accurate than competing devices, this enables accurate monitoring of supply voltages lower than 1.8V where a high accuracy power supply is needed. The externally resistor programmable inputs enable a power supply designer to have any power up sequence simply by choosing which supply goes into which input. User programmable time delays can be set using external capacitors. The device is also housed in a 10-pin MSOP (mini small-outline plastic) package making it the industry’s smallest quad sequencer.

“Analog Devices offers an innovative portfolio of sequencers with products capable of sequentially powering up from two to 10 supply rails,” said Pat Meehan, product line manager, Power System Management, Analog Devices. “As a result, ADI can address all of our customers’ power sequencing needs with products that simplify the monitoring, diagnosis and configuration of power supply rails in a variety of applications, including telecommunications infrastructure, data communications and storage.”

Intelligent Fault Response
The ADM1185 quad channel voltage monitor and sequencer is powered from 2.7 V to 5.5 V and is capable of monitoring up to four supplies at 0.8 percent accuracy. In case of a voltage fault, an intelligent fault response feature shuts down the power good output flagging a system fault to the main system controller. The system controller can then power down the supply rails in a pre-determined order to prevent system damage. In the case of a power supply failure on the first Vcc all outputs are switched off. In addition to the ADM1185, Analog Devices offers the ADM106x, ADM108x and ADM6819/20 voltage monitor and sequencer families, which support from 2 to 10 power supply rails.

Availability and Pricing
The ADM1185 is sampling now with full production scheduled for December 2006. The devices are priced starting at $1.20 per unit in 1,000-piece quantities and is specified over an operating temperature range of –40 degrees C to +85 degrees C.

About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

Editor's Contact Information:

Sue Martenson
781/937-1989
781/937-1078
sue.martenson@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close