Norwood, MA (04/08/2008) - Analog Devices, Inc., a global leader in high-performance semiconductors for signal-processing applications, today introduced two new analog multiplexers manufactured on ADI’s proprietary iCMOS™ (industrial CMOS) process technology. Available in space saving packages, the ADG1406 and ADG1407 multiplexers operate with ±5-V, +12-V, or ±15-V supplies, delivering the industry’s lowest on resistance. Their low on resistance and on resistance flatness make them ideal solutions for data acquisition and gain switching applications in which low distortion is critical.
About the ADG1406 and ADG1407 Multiplexers
The new multiplexers feature 10-ohm maximum on resistance, with less than 0.9-ohm variation over a ±10-V signal range. The 16-channel ADG1406 switches one of sixteen single-ended inputs to a common output; the 8-channel ADG1407 switches one of eight differential inputs to a common differential output. Both provide 33-V supply maximum ratings, rail-to-rail operation, and break-before-make switching action. Their iCMOS manufacturing technology ensures ultra low power dissipation.
Availability and Pricing
The ADG1406 and ADG1407 are sampling now and will be available in full production quantities in July 2008. The parts are offered in a 28-lead TSSOP (thin-shrink small-outline) package as well as a 32-lead, 5-mm × 5-mm LFCSP (lead-frame chip-scale) package. Both the ADG1406 and ADG1407 are priced at $4.81 per unit in 1,000-unit quantities. For more information, visit http://www.analog.com/pr/ADG1406 or http://www.analog.com/pr/ADG1407.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
iCMOS is a trademark of Analog Devices, Inc.
Linda Kincaid
781-937-1472
linda.kincaid@analog.com
Careers |
Contact ADI |
About ADI |
Investor Relations |
News Room |
About This Site |
Site Map|
简体中文 |
日本語 |
eNewsletters |
Analog Dialogue |
© 1995 - Analog Devices, Inc. All Rights Reserved
沪ICP备09046653号