ANALOG DEVICES ANNOUNCES INDUSTRY’S FASTEST 16-BIT ADC AT 250 MSPS

- ADI continues to set converter performance standard with new AD9467; enables advances in radar systems, spectrum analyzers and multi-carrier, multi-mode receiver designs for wireless infrastructure.

Norwood, MA (09/27/2010) - The industry’s fastest 16-bit ADC (analog-to-digital converter)--at 250 MSPS (mega samples per second)--was unveiled today by data converter market share leader* Analog Devices, Inc. (ADI). The AD9467 16-bit, 250 MSPS ADC operates on 35% less power at 25% higher sampling rate than any other 16-bit data converter, providing a new level of signal processing performance for test and measurement instrumentation, defense electronics, and communications applications where high resolution over a wide bandwidth is needed. The AD9467 delivers resolution and a fast sample rate while simultaneously achieving a high SFDR (spurious-free dynamic range) of up to 100 dBFs and SNR (signal-to-noise ratio) performance of 76.4 dBFS. The device’s SFDR of 90 dBFS up to 300 MHz analog input and 60-femtosecond rms (root mean square) jitter helps lower the signal chain bill of materials component count by allowing engineers to increase system performance at higher intermediate frequencies, thereby reducing the number of signal down-conversion stages. Download data sheet or order samples and evaluation boards.

Analog Devices: Industry's Fastest 16-bit ADC at 250 MSPS

“We needed a 16-bit, 250 MSPS data converter with 90 db of SFDR for one of our key customer's highly advanced, data acquisition systems,” said Brian Kimball, principal hardware engineer, Mercury Computer Systems, a leading provider of open, application-ready, multi-INT subsystems for the intelligence, surveillance and reconnaissance market “The AD9467 data converter was designed into this system because it met our customer’s SFDR, ENOB (effective number of bits), and power requirements. Analog Devices engineers worked with us as trusted advisors to provide early-access silicon and provided design support to enable the timely development of our prototype product.”

The AD9467 can be used with ADI’s AD9523/24 low-jitter clock generators and ADL5562 3.3 GHz ultra-low distortion RF/IF differential amplifier to provide a data conversion signal chain solution.

“The AD9467 converter is attractive to National Instruments because of its industry-leading combination of sample rate and resolution,” said Phil Hester, senior vice president of R&D, National Instruments, a leading global supplier of hardware and software for engineers. “We are currently developing a module based on the AD9467 for our NI FlexRIO product family, which couples this new data conversion performance point with FPGAs that can be programmed using NI LabVIEW software. The AD9467 helps us maintain leadership in providing innovative solutions for test and measurement, software-defined radio, medical imaging, and scientific research applications.”

AD9467 16-bit, 250 MSPS ADC Key Features and Benefits:

  • 16-bit resolution with high signal bandwidths up to 300 MHz enables advanced signal acquisition subsystems in common radio platforms, radar systems, and spectrum analysis.
  • On-chip IF (intermediate frequency) sampling circuit and buffered analog inputs optimize the AD9467 for the highest ENOB and ease of use.
  • High dynamic range over broad signal bandwidth enables software-defined radios for use with multiple standards, such as LTE/W-CDMA, MC-GSM (class 1) and CDMA.
  • Programmable full-scale input range allows trade-off between SNR and SFDR enabling the design of more sensitive radar systems with the ability to acquire and track smaller targets with better accuracy. See chart below.

Input Span SNR SFDR Analog Input Sample Rate
2.5 Vp-p 74.4 dBFs 90 dBFs 300 MHz 250 MSPS
2.0 Vp-p 74 dBFs 95 dBFs 170 MHz 250 MSPS
2.5 Vp-p 76 dBFs 100 dBFs 100 MHz 160 MSPS

Pricing, Availability, and Tools

Product Sample
Availability
Production
Release
Resolution
(Bits)
Sample
Rate
(MSPS)
Price
Each In
1,000
Packaging
AD9467-250 Now November
2010
16 250 $120 72-lead LFCSP
AD9467-200 Now November
2010
16 200 $100 72-lead LFCSP
AD9467-200EBZ Now November
2010
- - $300 per
unit in
single unit
quantities
-
AD9467-250EBZ Now November
2010
- - $300 per
unit in
single unit
quantities
-

Data Converter Design Tools: ADC Behavioral Models

Analog Devices’ ADIsimADC™ online analog-to-digital behavioral model accurately models the typical performance characteristics of many of ADI’s high-speed converters. The model faithfully reproduces the errors associated with both static and dynamic features such as AC linearity, clock jitter, and many other product specific anomalies. This tool requires no downloads and allows you to graph specific performance plots and select products. ADC Analyzer™ is a downloaded tool that runs the behavioral models and configures evaluation boards. VisualAnalog™ takes this concept further by allowing designers to customize their input signal and data analysis. An input signal can be constructed from sine waves, noise sources, and vector data to see how an ADC will perform in real-world conditions.

Data Converters: Bridging the Analog and Digital Worlds

More designers turn to Analog Devices than any other supplier for the high-performance conversion technology required to bridge the analog and digital worlds in myriad electronic systems. With the industry’s leading portfolio of ADCs (analog-to-digital converters) and DACs (digital-to-analog converters), Analog Devices’ converter products feature the right combination of sampling rates and accuracy with low noise, power, and price and small package size required by industrial, medical, automotive, communications, and consumer electronics. To view ADI’s ADC selection guide, visit http://www.analog.com/ADCsearch. For ADC drivers, visit http://www.analog.com/ADCdrivers. To view ADI’s DAC selection guide, visit http://www.analog.com/DACsearch.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

*Analog Devices, Inc. leads the worldwide data converter market with a 46 percent share, according to industry analyst firm Databeans, Inc. in its market research report titled “2010 Data Converters.” Analog Devices’ 46 percent share is larger than the combined market share of the nearest eight competitors.

Follow ADI on Twitter at Follow ADI on: http://www.twitter.com/ADI_News

To subscribe for Analog Dialogue, ADI’s monthly technical journal, visit: http://www.analog.com/library/analogDialogue/.

LabVIEW, National Instruments, NI and NI FlexRIO are trademarks of National Instruments. Other product and company names listed are trademarks or trade names of their respective companies.

Editor's Contact Information:

Bob Olson
781/937-1666

bob.olson@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close