ANALOG DEVICES’ LINEAR REGULATOR FAMILY, OPTIMIZED FOR NOISE-SENSITIVE PORTABLE APPLICATIONS, IS AVAILABLE IN THE INDUSTRY’S SMALLEST PACKAGE
ADI’s new ADP120, ADP121 and ADP130 LDOs deliver the right balance of excellent noise performance and very low quiescent current, allowing mobile electronics designers to quickly and cost-effectively distribute clean power rails to noise-sensitive systems.
Norwood, MA (09/25/2008) -
Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications, has introduced a family of high-performance LDO (low dropout) regulators that generates the low noise, low voltage supply rails and extended battery life required for superior performance in mobile handsets and other battery-powered devices. The ADP120 and ADP121 LDOs are available in the industry’s smallest wafer-level chip scale package (WLCSP), as well as a standard TSOT option, offering design flexibility for high-performance, small form factor handsets. Leveraging ADI’s more than 40 years of experience in analog design, the ADP120, ADP121 and ADP130 LDOs achieve very low levels of noise and power consumption, providing portable electronics designers with a power management solution optimized for their application needs.
“Low-power and low-noise operation are key design challenges for mobile device designers being tasked with adding new features and functions into power-sensitive consumer, industrial and medical devices,” said Arcadio Leon, marketing director for portable power products, Analog Devices. “Part of ADI’s growing portfolio of power management solutions, the ADP120, ADP121 and ADP130 LDO trio delivers an optimized balance of low quiescent current and low noise to improve performance and extend battery life.”
The new devices are part of a family of low-noise LDOs that provide clean power to noise-sensitive mixed-signal ICs with supply currents below 350 milliamps (mA), while consuming only 11 microamps (µA) to 24 µA of quiescent current (Iq) and operating at output voltages as low as 1.2 V. All three devices are stable with a very small 1 µF ceramic output capacitor, eliminating the need for additional bypass capacitors. This reduces the amount of board space required as well as the bill-of-materials cost. The combination of signal integrity and low-power operation allows designers of lithium-battery-powered devices, such as portable audio players, digital still cameras, handheld games and personal navigation systems, to quickly and cost-effectively resolve noise issues associated with dc power management. The very low Iq, along with a shutdown current in the nanoampere range, helps to reduce parasitic drain on the battery when the application is turned off, expanding the power budget to extend battery life or allow operation of other system functions.
The ADP120 and ADP121 feature 60 dB PSR (power supply rejection) at 10 kHz, while achieving noise figures of 40 µV rms and consuming only 11 µA , making them ideal to power RF and analog circuitry in portable applications. In addition, the ADP130 offers a unique dual-supply architecture that enables excellent low dropout performance when compared to single-supply devices. Leveraging this architecture, the ADP130 can be biased from a higher input supply, while the load current is sourced from a lower input supply to reduce overall power dissipation and enable low dropout operation.
The ADP120 and ADP121 LDOs feature a low 60-mV dropout voltage for 100 mA of load current. The ADP130 features an ultra-low 17-mV dropout voltage, making it ideal for generating low output voltages for small geometry digital cores and processors used in devices such as camera modules.
Availability and Pricing
The ADP120, ADP121 and ADP130 LDOs are available now in production quantities. In a 5 lead TSOT (thin, small-outline transistor) package, the ADP120 is $0.26, the ADP121 is $0.27 and the ADP130 is $0.33 in 1,000-unit quantities. The new ADP120 and ADP121 LDOs are also available in an ultra-small, 0.86 mm × 0.86 mm 4-ball WLCSP (wafer-level chip scale package) option. For WLCSP pricing information, please contact Analog Devices at
Power.Management@analog.com.
For more information on ADI’s new LDOs, www.analog.com/pr/ADP120. These products are supported by ADI’s online ADIsimPower™ design tool, which can be accessed at:
http://designtools.analog.com/dtPowerWeb/dtPowerMain.aspx.
About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
Editor's Contact Information:
Sue Martenson
781-937-1989
sue.martenson@analog.com