content here.
content here.

ANALOG DEVICES SETS NEW PERFORMANCE LEVEL WITH NEW FAMILY OF HIGH-DYNAMIC-RANGE, SINGLE-CHANNEL MIXERS

ADI Sets New Performance Level with New Family of High-Dynamic-Range, Single-Channel Mixers.

Norwood, MA (03/03/2009) - Adding to its broad portfolio of RF ICs, Analog Devices, Inc. (ADI), a world leader in high-performance semiconductors for signal-processing applications, today introduced a family of five single-channel RF mixers for high-dynamic-range applications within satellite communications, wireless base stations, point-to-point radio links, instrumentation, and military equipment.

Covering the 10-MHz to 6000-MHz range, the ADL5801 single-channel active mixer, which has the widest available operating frequency, complements the ADL5802 dual-channel active mixer announced in October 2008. The ADL5355, ADL5357, ADL5365 and ADL5367 high-performance, single-channel passive mixers, specified for operation across the cellular frequency ranges, complement the ADL5356, ADL5358, and ADL5360 dual-channel passive mixers.

ADL5801 Wideband Single-Channel Active Mixer
The ADL5801 mixer, the industry’s first broadband single-channel device to enable down- and up conversion of signals, is suitable for both transmit and receive signal paths. The industry’s highest linearity active mixer, the ADL5801 is packaged in a 4 mm × 4 mm LFCSP and consumes 50% less power than the competing passive devices. The ADL5801 single-channel active mixer achieves 27-dBm IIP3 (third-order input intercept point) with 10-dB single sideband noise figure. In addition, the ADL5801 provides a conversion power gain of 1.5 dB, reducing the need for an additional IF amplifiers.

Unique to the ADL5801, an on-chip input power detector can be used to adjust the mixer bias. This adaptive bias feature allows for optimal high IP3 performance when presented with large unwanted interferers, often referred to as blocking signals. When blockers are no longer present the ADL5801 automatically switches to a lower power operating mode.

ADL5355, ADL5357 Single-Channel Passive Mixers with integrated LO and IF Amplifiers
The ADL5355 mixer operates over the 1500 MHz to 2500 MHz frequency range; the ADL5357 mixer operates over the 500 MHz to 1500 MHz frequency range. With on-chip IF and LO amplifiers and input baluns, the mixers offer the highest level of integration. The ADL5355 and ADL5357 mixers achieve 27-dBm IIP3 with 8.1-dB power conversion gain, and 9.4-dB single-sideband noise figure. In high interference environments, where the noise figure must not be degraded due to blocking, both products provide best-in-class performance with better than 18 dB SSB noise figure in the presence of an 10-dBm blocker.

ADL5365, ADL5367 Single Passive Mixer with integrated LO Amplifier
The ADL5365 mixer operates over the 1500MHz to 2500 MHz frequency range; the ADL5367 mixer operates over the 500 MHz to 1500 MHz frequency range. Removing the IF amplifier allows the mixer to be configured for use as either an up- or down converter.

Achieving the industry’s lowest power conversion loss (–7 dB), the ADL5365 and ADL5367 mixers provide 31-dBm input IP3 and 7.1-dB SSB noise figure. Featuring the highest input linearity IP3 specifications, they are ideally suited for use in transmit path observation receivers, and other applications that operate with high input signal power.

No external components are required on the RF or LO inputs to achieve these best-in-class results, making them suitable for the highest performance integrated receiver down conversion applications requiring a high-gain mixer. Unlike competitive devices, the single-channel passive mixer family provides power-down functions, and operates over a 3.3-V to 5-V supply voltage range, making them suitable for power-sensitive applications.

Both new mixer families, manufactured on an advanced SiGe bipolar process, provide 2000 V HBM ESD, simplifying handling procedures as compared to sensitive GaAs mixers.

Availability and Pricing
The ADL5801, ADL5355, ADL5357, ADL5365 and ADL5367 mixers and evaluation boards are available to order in sample quantities. The ADL5801 is priced at $5.15; the ADL5355, and ADL5357 are priced at $6.98; and the ADL5365 and ADL5367 are priced at $5.99 in 1000-unit quantities. For more information, visit: http://www.analog.com/mixers-multiplexers.

ADI’s RF IC Portfolio Covers Entire RF Signal Chain
Using a unique combination of design skills, system understanding and process technologies, Analog Devices offers the broadest portfolio of RF ICs covering the entire RF signal chain from industry-leading high-performance RF function blocks to highly integrated single-chip transceiver solutions. The RF function blocks include DDS and PLL synthesizers; TruPwr™ power detectors and logarithmic amplifiers; X-Amp® VGAs; power amplifiers, LNAs and other RF amplifiers, mixers and direct conversion modulator and demodulator products. For more information, visit: http://www.analog.com/rf.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

Editor's Contact Information:

Colleen Cronin
781/937-1622

colleen.cronin@analog.com