content here.
content here.

ANALOG DEVICES SPEEDS “SMART CAMERA” DEVELOPMENT WITH NEW DIGITAL VIDEO REFERENCE DESIGN

- Blackfin® running uClinux™ OS provides a broad range of capabilities from basic security monitoring to advanced video analytics

Norwood, MA (03/30/2009) - Analog Devices, Inc. (ADI) announces the availability of a complete IP surveillance and machine vision camera reference design based on the company’s Blackfin BF526C processor. The reference design, which aims to help engineers quickly develop and customize “smart camera” designs, implements a complete IP video camera, including the camera lens and a D1/HD1/CIF resolution image sensor.

“This design contains all of the functionality for an advanced, networked digital camera,” said Michael Long, Product Line Manager for Industrial Video and Imaging Solutions in Analog Devices’ General Purpose DSP Division. “The performance of the Blackfin solution enables a range of capabilities from basic monitoring to those found in today’s advanced ‘smart camera’ products.”

Aimed primarily at engineers developing security surveillance and machine-vision applications, the reference design includes a Blackfin processor running the uClinux™ operating system. The BF526C provides a convergent solution in a unified core architecture that allows video signal processing concurrent with RISC MCU processing to handle network interface demands. Powerful video and audio processing on a single convergent processor provides for a unified software development environment, faster system debugging and deployment, and lower overall system cost. The processor provides camera developers with an integrated audio codec (SSM2603 derivative), streaming video and IP protocols, on-chip DRAM memory, and interfaces for 10/100 Ethernet, USB and SD storage, as well as a native RS-232 port.

The reference design unit can capture video at CIF, VGA, and D1 resolutions at either 30 fps (NTSC) or 25 fps (PAL). The fully programmable Blackfin solution allows for numerous video compression standards such as H.264 and MPEG4 while the audio is encoded to the G.729 standard. The camera supports 2-way audio for communication from control centers to camera locations. Pan-Tilt-Zoom control is supported through either Pelo-P or Pelo-D protocol.

An optional daughter card with the dual-core BF561 processor is available, enabling the system to deliver increased video resolution, while providing headroom to perform advanced analytic processing on the video stream such as motion detection/tracking.

Availability
The IP camera reference design is available immediately in the U. S. through DigiLink Software of Irvine CA, a leading supplier of IP-based digital media software and turnkey solutions. Beijing Emvideo Technology Co, Ltd is distributing and supporting the new design in Asia. European support is available through Cynove.

A Convergent Future Demands Blackfin-Class Processing
Analog Devices’ Blackfin embodies a new breed of 16/32-bit embedded processor with the industry’s highest performance and power efficiency for applications where a convergence of capabilities -- multi-format audio, video, voice and image processing; and real-time security and control processing -- are critical. It is this powerful combination of software flexibility and scalability that has gained Blackfin widespread adoption in convergent applications such as digital home entertainment, networked and streaming media, automotive telematics and infotainment, and digital radio and mobile TV.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

Blackfin is a registered trademark of Analog Devices, Inc. All other trademarks included herein are the property of their respective owners.

RSS Feed: http://www.analog.com/processors/news/pressreleases/index.html.

Editor's Contact Information:

Jessen Wehrwein
781/461-3337

jessen.wehrwein@analog.com