Norwood, MA (02/23/2011) - Analog Devices, Inc. (ADI), a global leader in semiconductors for high-performance signal processing applications and RF ICs (radio frequency integrated circuits), today introduced a highly integrated, low-power RF transceiver for operation in the global 2.4 GHz ISM (industrial, scientific and medical) frequency band. As the latest addition to ADI's extensive RF IC product portfolio, the ADF7241 RF transceiver is designed with emphasis on flexibility, ease-of-use characteristics, and low power consumption. The highly integrated ADF7241 RF transceiver enables support of the standard IEEE 802.15.4 PHY protocol at 250 kbps on a single chip. The transceiver's low-power consumption of 19mA in receive mode and 21.5 mA in transmit mode makes it effective for battery-powered systems, such as wireless sensor networks, automatic meter reading, industrial wireless control, wireless audio and video, consumer electronics, and ZigBee® applications.
The receive path of the ADF7241 RF transceiver is based on a zero-IF architecture enabling best-in-class blocking and high selectivity performance, while the transmit path is based on a closed loop VCO (voltage controlled oscillator) modulation scheme, which provides a high modulation quality. It also features a flexible port RF-interface with support for switched antenna diversity. In order to optimize the system power consumption, the ADF7241 RF transceiver incorporates a robust, very low-power, custom 8-bit processor that supports a number of RF functions, including radio control and packet management. The integrated 8-bit processor is firmware that can be programmed to execute firmware modules or system upgrade patches from internal RAM memory, which provides the flexibility to respond to protocol standard evolution and maintain system robustness.
The ADF7241 RF transceiver is equipped with a SPI (serial port interface) for high throughput efficiency as well as a bi-directional SPORT (serial port). The transceiver can be easily designed into system designs with ADI's ADSP-21xx, SHARC®, TigerSHARC® , and Blackfin® Processors.
| Product | Price Each In 1,000-unit Quantities | Availability | Packaging |
|---|---|---|---|
| ADF7241 | $1.98 | Now | 32-lead LFCSP |
Using a unique combination of design skills, system understanding and process technologies, Analog Devices offers the broadest portfolio of RF products covering the entire RF signal chain from industry-leading high-performance discrete RF function blocks to highly-integrated multi-functional single-chip RF solutions. These products are also supported by a wide range of free design tools, evaluation boards and other design resources to ease the development of RF systems. For more information, visit: http://www.analog.com/rf.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Blackfin, TigerSHARC, SHARC are registered trademarks and ADIsimSRD is a trademark of Analog Devices. All other trademarks included herein are the property of their respective owners.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
Colleen Cronin
781-937-1622
colleen.cronin@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved