INDUSTRY’S SMALLEST DUAL BUCK REGULATOR REDUCES COMPONENT COUNT AND BOARD SPACE IN PORTABLE SYSTEMS

- ADI’s ADP5022 dual step-down regulator with on-chip LDO is half the size of other multi-output converters, eliminating up to 12 discrete components from handheld instrumentation equipment and mobile devices.

Norwood, MA (12/16/2009) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications, today introduced the industry’s smallest dual buck (step-down) regulator for space-constrained portable electronic systems. At just 2 mm × 2 mm × 0.6 mm, the dual 600-mA (milliamp) ADP5022 high performance step-down converter is half the size of competing devices yet includes an additional 150-mA on-chip LDO (low dropout regulator), a convenient feature for powering auxiliary rails. The high level of integration and small package size enables a cost-effective, ultra-small, power management unit for portable instruments, smart energy meters, smart phones and other power-sensitive equipment that requires thin packages. The combination of small size, low-noise architecture and high switching frequency also make the ADP5022 ideal for powering sensitive analog circuits like high-resolution ADCs (analog-to-digital converters).

The 3-MHz (megahertz) regulators included in the ADP5022 provide fixed-voltage outputs and internal compensation, delivering exceptional efficiency and performance while minimizing the external filter size and eliminating as many as 12 discrete components from system board design. To maintain high efficiency at both light and heavy loads, the ADP5022 automatically shifts between PWM (pulse-width modulation) mode and PSM (power-save mode). The MODE pin can be used to force the device into PWM mode across all loads.

The ADP5022 provides important features that help enable the design of high efficiency noise sensitive analog and RF systems. A key to designing sensitive analog circuits is getting the regulator physically close to the load. The compact size of ADP5022 allows the system designer to place the power regulation right alongside the point of load, minimizing PCB parasitics. The buck regulators employ a low-noise driver technique, high switching speed and out of phase clocking to further reduce noise. These features, along with the integrated high PSRR LDO, provide an ideal solution to power high-performance analog and digital loads (high-speed, high-resolution data converters, for example).

ADP5022 Key Features and Benefits

  • Small 2 mm × 2 mm 16-lead WLCSP package
  • Dual buck regulators feature current mode architecture for excellent transient response
  • Out-of-phase operation for reduced input filtering
  • Low-noise driver architecture for lower high-frequency switching content
  • Low, 24-μA typical quiescent current per channel, no switching
  • 150 mA LDO enables auxiliary analog rail
  • High PSRR (power supply rejection ratio) of 60 dB up to 10 kHz
  • Low 65 μV rms output noise at VOUT3 = 3.3 V
  • Availability and Pricing

    Product Samples Availability Temperature
    Range
    Price Each
    per 100,000
    Packaging
    ADP5022 Now Now −40°C to +125°C $0.65 2 mm × 2 mm,
    16-lead WLCSP

    For more information, visit http://www.analog.com/pr/ADP5022. For more information on ADI’s integrated multi-output regulator portfolio, visit http://www.analog.com/pr/multi-output-regulators. To connect with a specialist, cross reference tools, and for more resources on how to use and obtain ADI products, please click here: http://www.analog.com/buy.

    ADI in Power Management
    Analog Devices brings world-class signal-processing prowess to a portfolio of innovative power-management ICs that complement high-performance signal-processing functions in a wide range of portable and fixed-power applications in consumer electronics, medical equipment, industrial and instrumentation, and communications infrastructure. By supporting signal-chain design requirements, such as dynamic range, transient performance, and reliability, ADI helps customers solve complex power challenges easily and quickly, differentiate their products, and get to market faster. Learn more about ADI's power-management ICs at http://www.analog.com/power.

    About Analog Devices

    Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

    Subscribe to ADI’s News Feed.

    Follow ADI on: http://www.twitter.com/ADI_News.

    Editor's Contact Information:

    Howard Wisniowski
    781/937-1517

    howard.wisniowski@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close