MOSFET DRIVERS IMPROVE EFFICIENCY WITH HIGH SWITCHING SPEEDS AND OVERTEMPERATURE PROTECTION

- Analog Devices’ ADP36xx family of 18-volt MOSFET drivers provides 2-A and 4-A peak currents with best-in-class propagation delays and edge rise and fall times for power conversion and control designs.

Norwood, MA (11/19/2009) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications, today announced a family of new high-speed 18-volt MOSFET drivers that provide 2-A (amps) and 4-A peak currents. Among the industry’s fastest, they feature propagation delays of 14 ns to 35 ns (nanoseconds) and edge rise/fall times of 10 ns to 25 ns. The new ADP36xx MOSFET driver family improves system reliability with the inclusion of overtemperature protection, UVLO (undervoltage lockout) and precision shutdown capability. The drivers can be used to complement PWM (pulse width modulation) controllers, such as ADI’s award-winning ADP1043A digital controller, improving system efficiency, while enabling high switching frequencies in isolated power conversion and motor control systems.

These new high-current, high-speed, dual 18-volt drivers are capable of driving two independent N-channel power MOSFETs. Using industry-standard packages, the parts have an internal temperature sensor and provide two levels of overtemperature protection: warning and shutdown at extreme junction temperatures. The shutdown function, generated from a precise internal comparator, provides fast system enable or shutdown, allowing redundant overvoltage protection and complementing the protection function of the switching controller. A wide input voltage range allows the drivers to be compatible with both analog and digital PWM controllers. Digital power controllers are powered by a low voltage supply, while the drivers are powered by a higher voltage supply. UVLO and hysteresis functions allow safe startup and shutdown of the higher voltage supply when used with low-voltage digital controllers. The device families are available in thermally enhanced SOIC_EP (small outline package with exposed pad) and Mini SO_EP (mini small outline package with exposed pad) packaging to maximize high frequency drive capability in a small PCB (printed circuit board) area.

Key features and benefits of the ADP36xx family of high-speed MOSFET drivers:

  • Up to 18-volt input, making them ideal for 12-volt power supplies.
  • High-speed switching provides low propagation delays and fast edge rise and fall times for improved efficiency and high-frequency operation.
  • Overtemperature warning and shutdown features provide improved system safety and protection.
  • Precision shutdown functionality provides backup protection against catastrophic failures and damage.
  • UVLO functionality guarantees drive integrity in all start-up and shutdown scenarios.

Availability and Pricing

Product
Samples
Availability
Supply Voltage (V)
Temperature Range Ambient
Price Each Per 1000
Packaging
ADP3623
NOW
NOW
4.5 to 18
−40°C to +85°C
$0.94
$0.88
Mini_SO_EP
SOIC_EP
ADP3624
NOW
NOW
4.5 to 18
−40°C to +85°C
$0.94
$0.88
Mini_SO_EP
SOIC_EP
ADP3625
NOW
NOW
4.5 to 18
−40°C to +85°C
$0.94
$0.88
Mini_SO_EP
SOIC_EP
ADP3629
NOW
NOW
9.5 to 18
−40°C to +85°C
$0.84
$0.78
Mini_SO
SOIC_EP
ADP3630
NOW
NOW
9.5 to 18
−40°C to +85°C
$0.84
$0.78
Mini_SO
SOIC
ADP3631
NOW
NOW
9.5 to 18
−40°C to +85°C
$0.84
$0.78
Mini_SO
SOIC
ADP3633
NOW
NOW
9.5 to 18
−40°C to +85°C
$0.88
$0.96
Mini_SO_EP
SOIC_EP
ADP3634
NOW
NOW
9.5 to 18
−40°C to +85°C
$0.94
$0.88
Mini_SO_EP
SOIC_EP
ADP3635
NOW
NOW
9.5 to 18
−40°C to +85°C
$0.94
$0.88
Mini_SO_EP
SOIC_EP

ADI in Power Management
Analog Devices brings world-class signal-processing prowess to a portfolio of innovative power-management ICs that complement high-performance signal-processing functions in a wide range of portable and fixed-power applications in consumer electronics, medical equipment, industrial and instrumentation, and communications infrastructure. By supporting signal-chain design requirements, such as dynamic range, transient performance, and reliability, ADI helps customers solve complex power challenges easily and quickly, differentiate their products, and get to market faster. Learn more about ADI's power-management ICs at http://www.analog.com/power.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

Subscribe to ADI’s News Feed.

Follow ADI: http://www.twitter.com/ADI_News.

Editor's Contact Information:

Howard Wisniowski
781/937-1517

howard.wisniowski@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close