Norwood, MA (11/05/2008) - Analog Devices, Inc. (NYSE: ADI), the global leader in data conversion technology, is helping electronic equipment manufacturers design more energy-efficient products with the introduction today of eight TxDAC® transmit digital-to-analog converters (DACs), each integrating two DACs on a single device. Adding to ADI’s extensive high-speed DAC portfolio, the new pin-compatible dual TxDAC converters are designed for communications, industrial, instrumentation and other demanding high-performance applications for which low power consumption and space savings yield significant cost, performance and time-to-market advantages. Dissipating only 220 mW at their maximum sample rate, the AD911x series of dual TxDAC devices consume 40 percent less power and are one-third the size of competing transmit DACs, while achieving 10 dB better SFDR (spurious-free dynamic range) performance. The AD971x series of dual TxDAC devices, with 2-mA full-scale output current, are even more energy efficient, consuming 70 percent less power than competing solutions.
“With the industry increasingly focused on efficiency and portability, design engineers are being squeezed to reduce power consumption and board space in their designs,” said David Robertson, product line director for the High Speed Signal Processing group, Analog Devices. “Whether they’re designing femtocell base stations, battery-powered instrumentation or medical applications, designers are looking for new DAC products that will help them meet their space and power budgets, without sacrificing performance.”
Low Power, Integration and Flexibility
Each new TxDAC integrates two 14-, 12-, 10- or 8-bit digital-to-analog converters with sample rates up to 125 MSPS (mega-samples-per-second). These devices allow designers to adjust the full-scale current from 1 to 4 mA or 4 to 20 mA with a single, pin-compatible architecture and common software code.
The AD971x TxDAC series features 1- to 4-mA maximum differential output current. Power dissipation at 2 mA output current is only 37 mW at 10 MSPS and 53 mW at 50 MSPS. This is one-third that of competing transmit DACs, making the new series ideal for small, limited range wireless equipment, such as picocell and femtocell base stations and battery-powered medical, industrial and instrumentation applications.
The AD911x TxDAC series has 4- to 20-mA maximum differential output current. It dissipates 40 percent less power than other devices in its class and is suited to automotive, medical, instrumentation and communications applications where channel densities must be maximized without the addition of cooling fans or where environmental considerations are driving a reduction in power consumption. The AD911x devices achieve 85-dB SFDR to 10 MHz, which is superior to other devices in its class.
Despite their small 6 mm x 6 mm package size, the new DACs are loaded with performance features, such as an internal calibrator for improved INL and DNL performance up to a 10-MHz output frequency, an internal voltage reference, independent full-scale current control, on-chip load and common-mode resistors, and a pair of auxiliary DACs that can be used for generating control voltages or for system calibration.
The new TxDAC devices offer a seamless interface to ADI’s high-performance quadrature modulators, such as the ADL5370. If a single-ended or differential-buffered voltage output is needed, then the ADA4899-1 and ADA4841-2 operational amplifiers are excellent choices, respectively. Additionally, Analog Devices’ high speed converters, such as the AD911x TxDAC family, are designed to operate seamlessly with ADI’s AD9513 clock distribution IC and new line of voltage regulators, including the ADP3334 and ADP3333.
Pricing and Availability
The TxDACs are available now in volume production. The devices come in a small, 6 mm × 6 mm, Pb-free, 40-lead LFCSP (lead-frame chip-scale package). For more information, visit http://www.analog.com/pr/AD971x.
| AD9117BCPZ | |||
| AD9116BCPZ | |||
| AD9115BCPZ | |||
| AD9114BCPZ | |||
| AD9717BCPZ | |||
| AD9715BCPZ | |||
| AD9714BCPZ |
Industry’s Leading Converter Portfolio
More designers turn to Analog Devices than any other supplier for the high-performance conversion technology required to bridge the analog and digital worlds in today’s myriad electronic systems. With the industry’s leading portfolio of analog-to-digital converters and digital-to-analog converters, Analog Devices’ converter products feature the right combination of sampling rates, accuracy and reduced noise, power dissipation, price and package size required in industrial and instrumentation, medical equipment, automotive systems, communications infrastructure, and consumer electronics. Evaluation tools help customers quickly validate, select, and design in the optimal data converters to reduce design complexity, development schedules, and bill-of-material costs. To view ADI’s ADC selection guide, visit http://www.analog.com/ADCSearch. For ADC drivers, visit: http://www.analog.com/ADCDrivers. To view ADI’s DAC selection guide, visit http://www.analog.com/DACSearch.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
TxDAC is a registered trademark of Analog Devices, Inc.
For more information on ADI's most recent product releases, visit our Press Release home page.
Sue Martenson
781/937-1989
sue.martenson@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved