ANALOG DEVICES ANNOUNCES INDUSTRY’S FASTEST, 1NV/√HZ, LOW POWER, RAIL-TO-RAIL AMPLIFIERS

ADA4895-6-7

Norwood, MA (09/28/2011) - Analog Devices, Inc. (ADI) today unveiled a series of high-speed amplifiers that establish a new performance standard with the best combination of high-speed, low noise and low power. Designed for portable, multi-channel and low power instrumentation and healthcare equipment, the ADA4896-2 (dual), ADA4897-1(single) and ADA4897-2 (dual) high-speed amplifiers provide the highest large-signal bandwidth and slew rate with the lowest noise available today in a rail-to-rail amplifier under 10 mW. Each amplifier features low noise of 1 nV/√Hz and 120-V/µs slew rate while consuming only 3 mA of supply current. Further, the 1/f noise @10Hz is a low 2.4 nV/√Hz. Watch this video and learn more about ADI's new series of high-speed amplifiers.

Also announced as part of this high-speed amplifier series was the ADA4895-2 dual de-compensated high-speed amplifier. It delivers 1.5-GHz gain-bandwidth product at gains of +10 and greater, making it ideal as a high-speed, high-gain pre-amplifier.

The new rail-to-rail amplifiers operate across the extended industrial temperature range of -40˚C to +125˚C and offer a 3-V to 10-V supply range. The ADA4895-2 and ADA4897-1/ -2 include an output disable feature.

Amplifiers Key Features

  • Low wideband noise: 1 nV/√Hz
  • Low 1/f noise: 2.4 nV/√Hz @ 10 Hz
  • Low distortion: −115 dBc @ 100 kHz, Vo= 2 V p-p
  • Low power: <3 mA
  • High speed
    • ADA4896-2, ADA4897-1, ADA4897-2
      • 230 MHz small signal bandwidth
      • 35 MHz large signal bandwidth
      • 120 V/μs slew rate
    • ADA4895-2 (de-compensated)
      • 1.5-GHz gain-bandwidth product (gain ≥+10)
      • 500-V/µs slew rate

Availability, Pricing and Complementary Components

Product Features Availability Price Each Per 1,000 Packaging
ADA4897-1 Single, Disable Full Volume Production $1.89 8-lead SOIC
6-lead SOT
ADA4897-2 Dual, Disable Samples Now $3.20 10-lead MSOP
ADA4896-2 Dual Full Volume Production $3.20 8-lead LFCSP
8-lead MSOP
ADA4895-2 Dual, Disable (Gain ≥+10) Samples Now $3.20 10-lead MSOP

Complementary components for these amplifiers include the AD7982 18-bit A/D converter and the AD9279 octal (eight-channel) ultrasound receivers. Find additional high-speed low noise amplifiers at http://www.analog.com/en/high-speed-op-amps/low-noise-low-distortion-amplifiers/products/index.html.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

To subscribe to ADI's News Feed http://www.analog.com/en/homepage/news.xml

Follow ADI on Twitter at http://www.twitter.com/ADI_News

To subscribe to Analog Dialogue, ADI’s monthly technical journal, visit: http://www.analog.com/library/analogDialogue/

Editor's Contact Information:

Bob Olson
781-937-1666

bob.olson@analog.com

content here.
content here.