PROGRAMMABLE LOW-POWER GPIO/KEYPAD CONTROLLERS SIMPLIFY INTERCONNECT CIRCUITS FOR LARGE QWERTY KEYPADS

ADP5589

Norwood, MA (08/24/2011) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal processing applications, introduced today the ADP5585 and ADP5589 GPIO (general-purpose input/output) port expander and keypad matrix controllers for devices that require expanded I/O lines or mechanical keypads up to QWERTY size. The new GPIO/keypad controllers feature the industry's lowest active current drain and integrated programmable logic/PWM (pulse-width modulator) in the smallest available package. These GPIO/keypad controllers save battery life in portable devices by consuming less than 30 µA (typical) when keys are pressed and less than 1 uA (typical) when the keys are idle.

The ADP5585 and ADP5589 simplify interface connectors by saving up to 10 I/O lines (ADP5585) and 19 I/O lines (ADP5589) to the main processor. Both keypad controllers support multiple, simultaneous key press detection and communicate presses and releases in a chronological order via a 16-byte FIFO. In addition to the built-in programmable logic devices, two programmable reset generators allow designers to program keys, GPIOs, and/or logic changes to generate a reset signal to restart a locked up processor. Both devices are available in small LFCSP (ADP5585: 3.0 mm × 3.0 mm; ADP5589: 3.5 mm × 3.5 mm) and WLCSP packages (ADP5585: 1.59 mm × 1.59 mm; ADP5589: 1.99 mm × 1.99 mm).

  • Learn more about the software drivers: Linux software drivers
  • View discussions and FAQs on Analog Devices’ Power Management products on Engineer Zone

The ADP5585 and ADP5589 are designed for devices with front-panel keypads that need to expand the number of GPIO ports without increasing pin count. Both devices free up the main processor from having to monitor the keypad, thereby reducing power consumption and increasing processor bandwidth for other functions. The new controllers handle all key scanning and decoding functions and use an interrupt line to flag the main processor when new key events have occurred. Both the ADP5585 and ADP5589 are equipped with FIFO registers that store up to 16 events which are then read back by the processor through an I2C -compatible interface. Evaluation boards and Linux software drivers are available to provide the necessary tools to implement new designs quickly and efficiently.

Key Features of the ADP5585 and ADP5589 GPIO/Keypad Controllers

  • Lower power consumption of 30 µA (typical) with keypad active, compared to 54 µA to 1000 µA available through alternative GPIO/keypad controllers
  • 16-event FIFO simplifies reading of key, GPIO, and logic changes
  • 10 configurable GPIO ports capable up to 30 keys can save up to 10 I/O lines to the main processor, simplifying interconnects (ADP5585)
  • 19 configurable GPIO ports capable up to 96 keys can save up to 19 I/O lines to the main processor, simplifying interconnects (ADP5589)
  • I2C interface with Fast-mode Plus (Fm+) supports data rates up to 1 Mbps

Availability and Pricing

Product Sample Availability Full Production Price Each Per 1,000 Packaging
ADP5585 Now Now $0.75 16-lead LFCSP
16-bump WLCSP
ADP5589 Now Now $1.20 24-lead LFCSP
25-bump WLCSP
ADP5585CP-EVALZ Now Now $160 Evaluation Board
ADP5589CP-EVALZ Now Now $160 Evaluation Board

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

Follow ADI on Twitter at http://www.twitter.com/ADI_News

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe.

All trademarks are the property of their respective owners

Editor's Contact Information:

Howard Wisniowski
781-937-1517

howard.wisniowski@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close