Norwood, MA (07/17/2012) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications, today introduced the ADP2441, DC-to-DC switching regulator, the most recent in ADI’s growing portfolio of integrated power management switching regulators. The new 36-V, 1-A (amp) step-down regulator integrates both low-on-resistance, high-side and low-side power switches to provide compact point-of-load design and offers more than 94 percent efficiency. Under light load conditions, the ADP2441 will automatically operate in PSM (pulse-skip mode) to reduce switching losses and improve energy efficiency.
The ADP2441 supports a wide input range from 4.5 V to 36 V to accommodate a diversity of point-of-load applications including industrial and communication equipment and healthcare electronics. Output voltage is adjustable from 0.6 V to 90 percent of input voltage. The new regulator also offers low minimum on-time of 50 ns (nano seconds) saving valuable board space and cost through its suitability for single-stage, high input to low output power conversion.
By using a current-mode constant frequency PWM (pulse-width modulation) control scheme, the ADP2441 offers excellent stability and transient response to minimize the output voltage ripple. The switching frequency of the regulator can be adjusted from 300 kHz to 1 MHz. The new regulator also offers precision enable, voltage tracking and power-good features to enable a simple and reliable start-up sequence. System reliability and protection are enhanced further through over-current protection, under-voltage lockout and thermal shutdown. The ADP2441 operates over the −40°C to +125°C junction temperature range and is available in compact 3 mm × 3 mm 12-lead LFCSP package. Analog Devices’ integrated power management switching regulators are also supported by the ADIsimPower™ design tools, which makes selecting components, simulating power supply performance and building evaluation circuits easy and fast.
| Product | Sample Availability | Full Production | Price each @ 1k units | Packaging |
|---|---|---|---|---|
| ADP2441 | Now | Now | $1.78 | 3 mm × 3 mm 12 lead LFCSP |
| ADP2441-EVALZ | Now | Now | $60.00 |
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
All trademarks are the property of their respective owners
Joe Dussi
781-937-1216
joe.dussi@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved