ANALOG DEVICES RELEASES TWO DUAL A/D CONVERTERS WITH LOWEST POWER/HIGHEST LINEARITY COMBINATION AVAILABLE

AD7902, AD7903 PulSAR® A/D converters provide robust, flexible, simultaneous sampling solutions for industrial applications.
Analog Devices Releases Two Dual A/D Converters with  Lowest Power/Highest Linearity Combination Ava

Norwood, MA (06/19/2014) - Analog Devices, Inc. (NASDAQ:ADI) introduced today two 16-bit, 1-MSPS A/D converters with pseudo differential and differential input options. The AD7902 dual pseudo differential and AD7903 dual differential PulSAR® A/D converters enable simultaneous or independent signal chain implementation to provide two sampling solutions in one package. Each A/D converter consumes 12 mW @ 1 MSPS, which is 70 percent less power than the closest competitor. Power consumption is scaled depending on throughput speed to address thermal dissipation challenges in dense data acquisition system designs. The A/D converters feature up to +/-0.5 LSB and 94 dB SNR for exceptional accuracy and precision making them ideally suited to a wide range of high performance multichannel applications including I/Q demodulation, motor and power control, automated test equipment, data acquisition and medical instrumentation.

  • Download AD7902 and AD7903 data sheet, order samples and evaluation boards
  • Connect with engineers and ADI product experts on EngineerZone™, an online technical support community

Both A/D converters incorporate a versatile serial interface port and are implemented as physically-isolated devices allowing for a robust signal chain design with functional safety considerations in mind. The physical isolation also allows verification and backup measurements enabling useful end-system fault detection.

Pricing and Availability

Product Sample Availability/Full Production Resolution Input Price Each Per 1,000 Packaging
AD7902 NOW 16-Bit Pseudo Differential $15 20-lead QSOP
AD7903 NOW 16-Bit Pseudo Differential $15 20-lead QSOP

The A/D converters can be designed into circuits for data acquisition applications with ADI’s ADA4841-1, ADA4941-1 or ADA4940 low-noise, low-distortion, rail-to-rail output amplifiers, the ADP7104 low-noise LDO and ADR4525 voltage reference series.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

PulSAR is a registered trademark and EngineerZone is a trademark of Analog Devices, Inc.

Follow ADI on Twitter

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe

Editor's Contact Information:

Grainne Murphy
+353 61-495540

grainne.murphy@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close