ANALOG DEVICES INTEGRATED 1-WATT, 2-STAGE DRIVER AMPLIFIERS COVER ENTIRE CELLULAR FREQUENCY RANGE

Norwood, MA (06/07/2011) - Analog Devices, Inc. (ADI), a world leader in high-performance semiconductors for signal processing applications and RF ICs (radio-frequency integrated circuits), today introduced two 1-watt, 2-stage RF driver amplifiers featuring the ability to cover the entire cellular frequency range used in wireless communications systems. The highly-integrated ADL5605 amplifier (covering the 700 MHz to 1000 MHz frequency range) and ADL5606 driver amplifier (operating in the 1800 MHz to 2700 MHz range) are pin-compatible, easy-to-tune and integrate two stages of gain, thereby saving significant board space when compared to traditional discrete designs. Furthermore, the new RF driver amplifiers integrate internal active biasing and a fast shutdown function for applications that require a power saving mode, or for applications such as wireless energy metering that transmit intermittently. These high-performance broadband RF driver amplifiers are well-suited for a variety of wired and wireless applications including cellular infrastructure; industrial, science, and medical- (ISM) band power amplifiers; defense and instrumentation equipment.

The ADL5605 and ADL5606 provide extremely flat gain and very high output third-order intercept (OIP3) specifications across their tuned frequency range. These features eliminate the need to compensate for gain loss elsewhere in the signal chain while enabling the signal strength to be increased, without compression, prior to the power amplifier stages. The ADL5605 provides an extremely flat gain of 23 dB, a P1dB of 31.1 dBm, an OIP3 of 44.3 dBm and a noise figure of 4.8 dB at 943 MHz. The ADL5606 provides an extremely flat gain of 23.8 dB, a P1dB of 30.7 dBm, an OIP3 of 45.7 dBm and a noise figure of 4.8 dB at 2140 MHz. Both amplifiers require few external components for tuning, making these amplifiers easy to implement in a wide variety of applications. Furthermore, the new RF driver amplifiers offer low power consumption as the ADL5605 draws only 312 mA and the ADL5606 draws only 360 mA on a single 5-V supply.

  • Stable over temperature, power supply and from device to device
  • Internal active biasing and a robust ESD rating of ±1 kV (Class 1C)
  • Fully specified for operation from −40°C to +85°C
  • Packaged in a compact 4-mm × 4-mm, 16-lead LFCSP that uses an exposed paddle for excellent thermal impedance
  • Fabricated on a GaAs HBT process

Product Price Each in
1,000 Quantities
Sample Availability Full Production Packaging
ADL5605 $7.75 Now June 2011 4-mm × 4-mm 16-lead LFCSP
ADL5606 $7.75 Now June 2011 4-mm × 4-mm 16-lead LFCSP

The ADL5605 and ADL5606 RF driver amplifiers can be designed into circuits for communications applications with ADI’s modulators with integrated PLL/VCO synthesizers including the ADRF6701, ADRF6702, ADRF6703, and ADRF6704.

RF IC Portfolio Covers Entire RF Signal Chain

Using a unique combination of design skills, systems understanding and process technologies, Analog Devices offers the broadest portfolio of RF products covering the entire RF signal chain from industry-leading high-performance discrete RF function blocks to highly-integrated multi-functional single-chip RF solutions. These products are also supported by a wide range of free design tools, evaluation boards and other design resources to ease the development of RF systems. For more information, visit: http://www.analog.com/rf.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

Follow ADI on Twitter at http://www.twitter.com/ADI_News.

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe

Editor's Contact Information:

Colleen Cronin
781-937-1622

Colleen.cronin@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close