Norwood, MA (05/10/2012) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications, today introduced a series of multipoint, low-voltage, differential signaling (M-LVDS) transceivers with the highest ESD (electrostatic discharge) protection of any multipoint LVDS transceivers. The ADN469xE M-LVDS series includes eight transceivers, each of which is capable of connecting 32 data/clock nodes using a single differential cable pair at data rates of 100 Mbps or 200 Mbps. Traditional LVDS communication links, by comparison, must use 32 separate point-to-point nodes, which significantly increases power, connector size, cabling costs and total board space. ADI’s ADN469xE M-LVDS series delivers 8 kV IEC ESD protection, offering up to 11 times the protection of competing M-LVDS transceivers. This higher level of protection improves the reliability of insertable/removable boards and cards used in wireless base station and networking infrastructure, data acquisition, automated test equipment and other high-speed, highly networked backplane and cable applications.
Available in half- and full-duplex versions, ADI’s ADN469xE transceivers are fully compliant with the TIA/EIA-899 M-LVDS standard. The new transceivers are available in configurations that include:
Availability and Pricing
| Product | Full Production | Receiver | Data Rate(Mbps) | Duplex | Price per 1k units | SOIC Packaging |
|---|---|---|---|---|---|---|
| ADN4690E | Now | Type 1 | 100 | Half | $1.05 | 8-lead |
| ADN4691E | Now | Type 1 | 200 | Half | $1.15 | 8-lead |
| ADN4692E | Now | Type 1 | 100 | Full | $1.05 | 14-lead |
| ADN4693E | Now | Type 1 | 200 | Full | $1.15 | 14-lead |
| ADN4694E | Now | Type 2 | 100 | Half | $1.05 | 8-lead |
| ADN4695E | Now | Type 2 | 100 | Full | $1.05 | 14-lead |
| ADN4696E | Now | Type 2 | 200 | Half | $1.15 | 8-lead |
| ADN4697E | Now | Type 2 | 200 | Full | $1.15 | 14-lead |
| EVAL-ADN469XEHDEBZ | Now | Half | $75.00 | |||
| EVAL-ADN469XEFDEBZ | Now | Full | $75.00 |
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe.
All trademarks are the property of their respective owners
Joe Dussi
781-937-1216
joe.dussi@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved