Norwood, MA (02/20/2013) - Analog Devices, Inc. (ADI) introduced today the AD5689R D/A converter. This16-bit dual nanoDAC+ continues the series of ADIs nanoDAC® products offering high performance in smaller packages. With relative accuracy of ±2-LSB INL, 2-ppm/°C 2.5-V reference, and space saving packages, this combination allows analog designers to address a wider range of applications without having to trade off performance for footprint. The series provides a straightforward pin compatible 10-bit to 16–bit upgrade/downgrade path for applications in a wide range of markets including communications infrastructure, industrial process control, healthcare and instrumentation.
The AD5689R also includes useful pin functions such as VLOGIC facilitating 1.8-V, 3-V and 5-V logic levels and a GAIN pin enabling the output range to be doubled. The series has both SPI and I2C interface options.
| Product | Sample Availability/Full Production | Resolution | Integrated Reference | Interface | Price Each Per 1,000 | Packaging |
|---|---|---|---|---|---|---|
| AD5689 | NOW | 16-bit | No | SPI | $4.18 | 16-lead LFCSP, 16-lead TSSOP |
| AD5689R | NOW | 16-bit | Yes | SPI | $4.48 | 16-lead LFCSP, 16-lead TSSOP |
| AD5697R | NOW | 12-bit | Yes | I2C | $2.80 | 16-lead LFCSP, 16-lead TSSOP |
| AD5687R | NOW | 12-bit | Yes | SPI | $2.80 | 16-lead LFCSP, 16-lead TSSOP |
| AD5687 | NOW | 12-bit | No | SPI | $2.50 | 16-lead LFCSP, 16-lead TSSOP |
| AD5338R | NOW | 10-bit | Yes | I2C | $1.96 | 16-lead LFCSP, 16-lead TSSOP |
| AD5313R | NOW | 10-bit | Yes | SPI | $1.96 | 16-lead LFCSP, 16-lead TSSOP |
The AD5689R can be designed into circuits for PLC, I/O cards applications with ADI’s AD5750-2 which is a single-channel, low cost, precision voltage/current output driver amplifier.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter
Subscribe to ADI's News Feed
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
Grainne Murphy
+353 61-495540
grainne.murphy@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved