content here.
content here.

ANALOG DEVICES MULTI-VOLTAGE MONITORS AND SEQUENCERS DELIVER INDUSTRY LEADING ACCURACY

ADI’s four-channel voltage monitor and sequencer ICs measure minute changes in processor voltage levels to prevent data loss and failures in high-availability communications infrastructure applications.
ADM1184

Norwood, MA (04/15/2008) - Analog Devices, Inc. (NYSE: ADI) is expanding its power management offerings with the industry’s most accurate low-voltage monitoring and sequencing ICs. Leveraging ADI’s precision analog design techniques, the new ADM1184 and ADM1186 quad voltage-monitor and sequencer ICs are twice as precise as competing devices, offering best-in-class accuracy (<±0.8%). The ADM1184 and ADM1186 also complete the industry’s only monitor and sequencer family to deliver <±1% accuracy for 2 to 12 supplies. The new ICs are designed for today’s advanced data and telecommunications infrastructure equipment, which is driven by extremely powerful processors with ever-lower core-voltage supplies. With unprecedented accuracy, the ADM1184 and ADM1186 precisely monitor processor cores to ensure they operate within voltage tolerance specifications, allowing power and system engineers to maximize system uptime and optimize system performance.

“As the operating level of ASICs, DSPs, FPGAs and other processing cores drops to 1 volt and below, the ability to reliably monitor low-voltage core supplies is becoming more difficult,” said John Perzow, marketing director for fixed power products, Analog Devices. “This creates the potential for under-voltage conditions that can result in lost data and system failure.”

By improving accuracy to less than ±0.8 percent, the ADM1184 and the ADM1186 meet today’s more demanding processor monitoring requirements, which promote safer, more reliable and better optimized system operation in sensitive, high-availability applications, such as wireless communications equipment. Competitive multi-voltage monitors and sequencers typically achieve a >± 1.5% accuracy level, which does not meet modern processor requirements for monitoring low-voltage core supplies with a low tolerance and narrow band of operation.

With industry-leading accuracy, a high level of functional integration, and a small package size, the ADM1184 and ADM1186 incorporate four precision comparators with 0.6-V references to monitor separate voltage rails. The new ICs operate on a 2.7-V to 5.5-V power supply and include four inputs that can be programmed to monitor different voltage levels using external dividers. Additionally, the ADM1186 allows power-up and power-down sequencing in hardware, eliminating the need for software support and further increasing system reliability by ensuring that the voltage supply rails are powered up and down in the correct order and within tolerance.

Availability and Pricing
The ADM1184 and ADM1186 are available now in production quantities. The ADM1184 is priced at $2.39 per unit in 1000-piece quantities and comes in a space-saving 10-lead MSOP (mini-small-outline package). The ADM1186-1 is priced at $3.80 per unit in 1000-piece quantities and comes in 20-lead QSSOP (quartersize small outline package). The ADM1186-2 is priced at $2.98 per unit in 1000-piece quantities and comes in a 16-lead QSSOP. Stand-alone and in-system application boards also are available to facilitate product evaluation. For more information, visit www.analog.com/pr/ADM1184 or www.analog.com/pr/ADM1186.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

Editor's Contact Information:

Sue Martenson
781-937-1989

sue.martenson@analog.com