Norwood, MA (04/21/2011) - Analog Devices, Inc. (ADI), released for general availability today the ADP8866 LED charge pump backlight driver which features independent control of nine LED current sinks, programmable LED blinking sequences and low operating current drain. Independent LED control allows designers to program different currents for each channel and enable them at different times. This feature allows the convenient control of backlighting LEDs and status indicator LEDs with one part. Programmable fade on/off and blinking sequences allow complex LED effects to be generated automatically, saving processor bandwidth and power. A built-in charge pump automatically adjusts its gain to efficiently power the LEDs under all conditions.
Requiring less than 1 µA during standby and less than 325 µA during automated blinking sequences, the ADP8866 programmable LED driver's low power consumption and simplified software interface make it an excellent choice for portable systems which require a high number of LEDs that need to be independently controlled. Such requirements are commonly found in keypad lighting, LCD lighting and analysis lighting applications. Evaluation boards are available, providing engineers with the necessary tools to implement their designs quickly and efficiently.
| Product | Sample Availability | Full Production | Price | Packaging |
|---|---|---|---|---|
| ADP8866 | Yes | Yes | $1.48 each per 1000 | 4 mm x 4 mm x 0.75 mm, 20-lead LFCSP |
| ADP8866CP-EVALZ | Yes | - | $120.00 each | - |
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe.
All trademarks are the property of their respective owners.
Howard Wisniowski
781-937-1517
howard.wisniowski@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved