Norwood, MA (04/18/2012) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications, today introduced the ADP2370/71 15-V, 800-mA output DC-to-DC regulator optimized for better energy efficiencies in battery-powered applications using multiple alkaline/NiMH, lithium cells, or other standard power sources.
The highly integrated ADP2370/71 regulators offer a wide input voltage supply range of 3.2 V to 15 V and require only three external components to reduce overall footprint. The ADP2370/71 offer greater than 93 percent conversion efficiency, enabling designers to support a higher load in a smaller area. During light load conditions, the ADP2370/71 can be configured to automatically switch to a low-quiescent power-save mode for additional battery life savings. The ADP2371, otherwise identical to the ADP2370, also offers a quick output discharge feature to ensure that the output bypass capacitors are completely discharged so that the processor can wake up in a known state.
By using a proprietary, high-speed, current-mode constant frequency PWM control scheme, the ADP2370/71 offer excellent stability and transient response to minimize the output voltage ripple. The switching frequency of these regulators can be synchronized to an external clock to eliminate beat frequencies between regulators. The ADP2370/71 operate over the −40°C to +125°C junction temperature range and are available in compact 3 mm × 3 mm QFN-8 lead packages.
| Product | Sample Availability | Full Production | Price each @ 1k units | Packaging |
|---|---|---|---|---|
| ADP2370 | Now | Now | $1.40 | 3 mm × 3 mm 8 lead LFCSP |
| ADP2371 | Now | Now | $1.40 | 3 mm × 3 mm 8 lead LFCSP |
| ADP2370CPZ-REDYKIT | Now | Now | $60.00 | - |
| ADP2371CPZ-REDYKIT | Now | Now | $60.00 | - |
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
All trademarks and registered trademarks are the property of their respective owners
Joe Dussi
781-937-1216
joe.dussi@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved