Norwood, MA (03/05/2010) - Lithium-ion (Li-ion) batteries are growing in popularity as energy storage reservoirs for high-voltage energy, industrial and automotive applications, such as wind turbines, photo-voltaic cells, and hybrid electric vehicles, and this has spurred demand for safer, higher performing battery monitoring and protection systems. Analog Devices, Inc. (NYSE: ADI), a global leader in high-performance semiconductors for signal-processing applications, has addressed the requirements of Li-ion battery manufacturers and power system designers with the unveiling today of a Li-ion battery monitoring and protection system that integrates all necessary components, including voltage and current measurement, signal isolation and safety monitoring.
Compared to NiMH (nickel-metal hydride) batteries, Li-ion batteries have a better energy-to-weight ratio, offer more efficient storage capacity over multiple charge-discharge cycles, and suffer less charge leakage when not in use. And unlike NiMH batteries traditionally used in high-voltage applications, battery stacks using Li-ion technology can comprise a large number of individual cells totaling hundreds of volts. Each cell must be properly monitored and balanced to ensure user safety, improve battery performance and extend battery life. ADI’s new Li-ion battery monitoring and protection system performs these functions while also allowing power system designers to replace costly discrete components, decrease power consumption and reduce system space.
“Li-ion batteries must be treated with respect. Fires have occurred in notebook computer applications because over-voltage peaks were not monitored correctly,” said Steve Sockolov, director, Precision Signal Processing group, Analog Devices. “Although the quality of battery fabrication has improved, guarding against higher temperature conditions in any energy, industrial or automotive application is critical. As one of the top suppliers to the energy, industrial and automotive industries, Analog Devices has the systems expertise and the right components to help customers with the design challenges associated with battery monitoring and safety.”
ADI offers the main components required for a complete Li-ion battery monitoring and protection system:
New Product: AD8280 Integrated Li-ion Battery Safety Monitor
The Li-ion battery monitoring and protection system includes a safety monitor, the AD8280, which Analog Devices also is launching today. The new safety monitor provides the designer with the final piece needed to develop the complete front-end of a battery monitoring and protection system. The AD8280 is an integrated solution that monitors six cell voltages and two temperature inputs. It is powered completely from the battery stack providing either a shared or a separate alarm for any of three conditions - over-voltage, over-temperature or under-voltage. Other benefits include:
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Subscribe to ADI’s News Feed.
Follow ADI on Twitter at http://www.twitter.com/ADI_News.
Bob Olson
781/937-1666
bob.olson@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved