ANALOG DEVICES' PROGRAMMABLE LED DRIVER ENABLES INDEPENDENT CONTROL OF NINE LED SINKS

ADP8866

Norwood, MA (04/21/2011) - Analog Devices, Inc. (ADI), released for general availability today the ADP8866 LED charge pump backlight driver which features independent control of nine LED current sinks, programmable LED blinking sequences and low operating current drain. Independent LED control allows designers to program different currents for each channel and enable them at different times. This feature allows the convenient control of backlighting LEDs and status indicator LEDs with one part. Programmable fade on/off and blinking sequences allow complex LED effects to be generated automatically, saving processor bandwidth and power. A built-in charge pump automatically adjusts its gain to efficiently power the LEDs under all conditions.

Requiring less than 1 µA during standby and less than 325 µA during automated blinking sequences, the ADP8866 programmable LED driver's low power consumption and simplified software interface make it an excellent choice for portable systems which require a high number of LEDs that need to be independently controlled. Such requirements are commonly found in keypad lighting, LCD lighting and analysis lighting applications. Evaluation boards are available, providing engineers with the necessary tools to implement their designs quickly and efficiently.

ADP8866 LED Backlight Driver Key Features and Benefits

  • Independent LED control allows different currents for each channel at different times.
  • Programmable fade on/off and blinking sequences automates complex fade and blinking sequences extending battery life and saving I2C bandwidth.
  • Automatic charge pump gain selection of 1X, 1.5X, and 2X enables maximum efficiency.
  • Available in LFCSP package reduces board space and simplifies board layout.

Availability and Pricing

Product Sample Availability Full Production Price Packaging
ADP8866 Yes Yes $1.48 each per 1000 4 mm x 4 mm x 0.75 mm, 20-lead LFCSP
ADP8866CP-EVALZ Yes - $120.00 each -

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

Follow ADI on Twitter at http://www.twitter.com/ADI_News

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe.

All trademarks are the property of their respective owners.

Editor's Contact Information:

Howard Wisniowski
781-937-1517

howard.wisniowski@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close