SINGLE 1500-MA LED FLASH DRIVER IMPROVES PICTURE QUALITY FOR CAMERA-ENABLED CELL PHONES

- With industry-leading efficiency and compact size, ADP1650 maximizes flash brightness in low light while minimizing battery current draw during flash events.

Norwood, MA (07/19/2010) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications, has introduced the ADP1650 1500-mA white LED driver – the latest addition to ADI’s power management portfolio and its inductive-based flash driver class of devices. The ADP1650 provides excellent flexibility with features like a programmable I²C-compatible interface, programmable torch and flash currents for one LED up to 1500 mA, two independent TxMASK1 inputs and a 4-bit ADC. The new LED driver also provides high efficiency at 85 percent at the typical battery voltage (90 percent peak) which reduces high levels of input battery current during flash and limits battery current drain in torch mode. The ultra-compact ADP1650 measures only 2 mm × 1.5 mm in a 12-ball WLCSP package and reduces PCB (printed circuit board) requirements.

“Camera quality is one of the most important features for consumers when selecting a handset, and since many camera phone images are taken spontaneously and in dimly lit areas or while talking on the phone, a quality flash is expected,” said Jose Rodriguez, technical director, Power Management Technology Group, Analog Devices.

The ADP1650 enables a complete high power flash design in less than 17 mm2 by integrating a programmable 1.5-MHz or 3.0-MHz synchronous inductive boost converter, a tiny, 1-mm high, low-cost, 1-μH power inductor, and 0603 case-size input and output capacitors. The new LED driver operates efficiently over the entire battery voltage range by maximizing the input-power-to-LED-power conversion and minimizing battery current draw during flash events. Designed to operate using the limited battery current available for flash, the ADP1650 connects easily to the latest image sensors and image processors to provide excellent picture quality in low ambient light environments. To download the data sheet, visit www.analog.com/pr/ADP1650ds.

Mr. Rodriguez added, “Maximizing light output for limited battery current and a shrinking PCB area is a key design challenge for portable device designers. The ADP1650 white LED driver meets this challenge.”

ADP1650 White LED Driver Features and Benefits

  • Ultra-compact 2 mm × 1.5 mm, 12-ball WLCSP package reduces PCB requirements
  • High efficiency at 85 percent at the typical battery voltage (90 percent peak) reduces high levels of input battery current during flash and limits battery current drain in torch mode
  • Two independent TxMASK (transmit mask) inputs permit the flash LED current and battery current to reduce quickly during a power amplifier current burst and protects the handset.
  • I²C-compatible interface enables the programmability of timers, currents, and status bit readback for operation monitoring and safety control

Availability and Pricing

Product Samples Availability Temperature
Range
Price Each
Per 1,000
Packaging
ADP1650 Now Now −40°C to +125°C $0.95 2 mm × 1.5 mm 12-bump WLCSP
ADP1650 Now Now −40°C to +125°C $0.95 3 mm x 3 mm 10-lead LFCSP (DFN)

For more information, visit www.analog.com/pr/ADP1650. For more information on ADI’s power-management products for White LED flash, visit http://www.analog.com/pr/LED.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

1) In a cell phone, Tx mask is used to quickly reduce the flash LED current and battery current during a power amplifier transmission burst. This feature allows for higher LED flash power because the PA burst during a flash event will not shut down the system.

Subscribe to ADI’s News Feed.

Follow ADI on: http://www.twitter.com/ADI_News.

Editor's Contact Information:

Howard Wisniowski
781/937-1517

howard.wisniowski@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close