ANALOG DEVICES UNVEILS ULTRA-LOW-POWER BOOST REGULATOR FOR ENERGY HARVESTING SYSTEMS

ADI’s ADP5090 offers low-light power conversion and multiple power path management capability.
Analog Devices Unveils Ultra-Low-Power Boost Regulator for Energy Harvesting Systems

Norwood, MA (04/01/2014) - Analog Devices, Inc. (NASDAQ: ADI) introduced today the industry’s most efficient ultra-low-power boost regulator for photovoltaic and thermoelectric energy harvesting systems. The ADP5090 ultra-low-power boost regulator represents a significant leap forward in energy harvesting technology by delivering efficient conversion of the harvested power (as low as 10 uW) with sub-uW operational losses that stores the maximum amount of energy for future operation. Harnessing “indoor” ambient light as a viable power source has become a growing trend in wireless sensor network applications worldwide.

  • Download ADP5090 data sheet, user guide or order samples
  • Connect with ADI engineers on EngineerZone™, an online technical support community

ADP5090 Ultra-Low-Power Boost Regulator Key Features

  • Optimizes efficient conversion of harvested limited power down to 10 µW – 1-mW range with best in class sub-µW operation losses
  • Programmable maximum power point tracking with open circuit voltage sensing ensures most energy extracted from harvester
  • 250-nA quiescent current in deep-sleep mode prolongs operation time with minimized loss of ambient energy
  • Integrated charge pump circuitry enables cold start at 380-mV input voltage with no energy on system node

Pricing and Availability

Product Availability Price Each per 1,000 Package
ADP5090 Now $2.50 3-mm x 3-mm 16-lead LFCSP

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

EngineerZone is a trademark of Analog Devices, Inc. All other trademarks are the property of their respective owners.

Follow ADI on Twitter

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe

Editor's Contact Information:

Joe Dussi
781-937-1216

joe.dussi@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close