Norwood, MA (01/19/2011) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal processing applications, introduced today the ADMP441 iMEMS® microphone, the industry's first high-performance MEMS microphone with an I2S (Inter-IC Sound) digital output. The ADMP441 also features an extended frequency response from 100 Hz to 15 kHz, high SNR (signal-to-noise ratio) of 61 dBA, and high PSRR (power-supply-rejection ratio) of 80 dBFS – features that have become the hallmarks of Analog Devices’ award-winning MEMS microphone portfolio. The new MEMS microphone uses patented ADI MEMS and audio signal processing technologies and is available in a thin 4.72 mm × 3.76 mm × 1.00 mm surface-mount package. It is reflow solder compatible with no sensitivity degradation. To download the datasheet, please visit http://www.analog.com/ADMP441
"For years, audio designers have been forced to design in additional signal processing in order to convert microphone output signals into standard I2S formats for non-mobile phone use. This increased both system cost and design complexity," said Kieran Harney, product line manager, MEMS/Sensors Technology Group, Analog Devices. "The innovative ADMP441 with industry standard I2S output offers plug–and-play use in a small footprint, simplifying audio system design while reducing overall signal chain cost and complexity. The ADMP441 is ADI's latest installment in a growing portfolio of high performance MEMS microphones that meet the demand for better sound quality and smaller footprints."
Additionally, the ADMP441 fully complies with the TIA-920 Telecommunications Telephone Terminal Equipment Transmission Requirements for Wideband Digital Wireline Telephones standard.
The ADMP441 iMEMS microphone is now sampling with volume production scheduled for June 2011. Pricing is $2.38 per unit in 1,000-unit quantities. For more information about Analog Devices' high performance iMEMS microphones, visit www.analog.com/mic.
Design engineers worldwide have become familiar with the vast capabilities of ADI's innovative iMEMS technology. The real promise of this technology is being realized daily in hundreds of cutting-edge applications, beginning with motion sensors and now with MEMS microphones. Combining nearly 20 years of MEMS know-how with ADI's audio signal processing expertise, iMEMS microphones provide unprecedented performance. iMEMS microphones and their many performance advantages will differentiate and radically change acoustic input designs in future electronics devices. For more information, visit www.analog.com/mic.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
iMEMS is a registered trademark of Analog Devices, Inc.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/library/analogDialogue/
Howard Wisniowski
781-937-1517
howard.wisniowski@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved