ANALOG DEVICES’ TACTICAL GRADE GYROSCOPE SENSORS ADD A NEW DIMENSION OF PERFORMANCE TO INDUSTRIAL DESIGN

- ADI’s latest iSensor® gyro and IMU provide full-factory calibration and exceptional stability control in robotics, navigation systems, and other industrial instrumentation applications.
ADIS16135 and ADIS16385, two highly integrated and precise MEMS inertial sensors

Norwood, MA (06/09/2010) - Industrial system designs involving platform stability, navigation, or precision measurements and diagnostics rely on multiple sensor inputs. In extreme environments where shock, vibration, and wide temperature ranges are present, a reliance on multiple sensor types or redundant sensors to compensate for environmental instabilities is common. System design engineers are under growing pressure to reduce this added system complexity and cost within existing and new applications. Analog Devices, Inc. (NYSE: ADI) is helping industrial equipment manufacturers more easily implement stabilization, navigation, and control features by adding two highly integrated and precise MEMS inertial sensors to its product line of iSensor® motion sensor products. The new sensors combine tactical grade (< 10 degrees per hour) gyroscope performance with ADI’s award-winning iSensor integration and factory calibration.

The ADIS16135 iSensor precision angular rate gyro and the ADIS16385 iSensor six-degrees-of-freedom inertial measurement unit (IMU) are both based on ADI’s iMEMS® (integrated Micro Electro Mechanical System) inertial sensor technology cores and offer an unmatched 6 degrees per hour bias stability, and angular random walk of 0.75 degrees/√hr. Extensive factory calibration results in an unmatched sensitivity of 16 ppm/degrees C and bias stability to within 0.003 degrees per second over -40 to 85 degrees C. The sensors are dynamically compensated and provide a simple user interface and control via a standard SPI (serial peripheral interface) and register interface. The ADIS16135 gyro and ADIS16385 IMU are designed for a broad range of industrial and instrumentation applications including: camera stability; antenna alignment; down-hole drilling; and GPS navigation in ships, aircraft, fleet vehicles, agricultural machinery and factory robotics.

“With tactical grade gyro performance available in ADI’s newest iSensor motion sensor products, complex stabilization and GPS-aided dead-reckoning is more easily enabled,” said Bob Scannell, iSensor business development manager, Analog Devices. “For industrial system designers who require the highest levels of gyroscope bias accuracy in extreme environments, the ADIS16135 gyro and ADIS16385 multi-axis IMU achieve the best cost-performance ratio available today.”

More About The ADIS16135 iSensor Gyroscope
The ADIS16135 is a high-performance single-axis digital gyroscope with a ± 300 degrees per second measurement range, a low noise level of 0.0122 degrees per second/√hr, and operates over a wide 335-Hz bandwidth using a single 4.85-V to 5.15-V voltage supply. The device is factory calibrated for temperature and voltage drift and provides superior linear acceleration sensitivity of only 0.03 degrees per second/g. It is also interface-compatible with all iSensor products, including the ADIS16385 IMU and others in the ADIS1636X series, further simplifying customer integration and migration plans. To download the data sheet, visit www.analog.com/pr/ADIS16135ds.

More About The ADIS16385 Six-degrees-of-freedom IMU
The ADIS16385 is a complete inertial measurement unit that includes a ± 300 degrees per second tri-axis gyroscope and a ±5-g tri-axis accelerometer. Tactical grade performance of 6 degrees per hour is available on the z axis gyro, with inertial grade performance provided on the x and y axis, providing a balanced price-performance solution for those applications with a primary axis of concern. The ADIS16385 IMU and the ADIS16135 gyro contain user-configurable internal filtering and multiple condition-monitoring options. To download the data sheet, visit www.analog.com/pr/ADIS16385ds.

Pricing, Availability and Compatibility
The ADIS16135 gyro and the ADIS16385 IMU are interface-compatible with current-generation IMUs, such as ADI’s ADIS1635x, ADIS1636x and ADIS1640x. Both devices operate over the temperature range of -40 to +105 degrees C.

Product Availability Operating Temperature
Range
Price Each
Per 1,000
Packaging
ADIS16135 In Volume
Production
-40° C to +105° C $499.00 36 mm x 44 mm x 14 mm
module package
ADIS16385 Sampling -40° C to +105° C $869.00 36 mm x 47 mm x 39 mm
module package
For more information on the ADIS16135 angular rate gyro, visit http://www.analog.com/pr/ADIS16135. For more information on the ADIS16385 IMU, visit http://www.analog.com/pr/ADIS16385.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

iSensor and iMEMS are registered trademarks of Analog Devices, Inc.

Subscribe to ADI’s News Feed.

Follow ADI on Twitter at http://www.twitter.com/ADI_News.

Editor's Contact Information:

Howard Wisniowski
781/937-1517

howard.wisniowski@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close