ANALOG DEVICES' IMEMS DUAL-AXIS ACCELEROMETER DELIVERS GUARANTEED HIGH TEMPERATURE OPERATION UP TO +175° C

ADI’s ADXL206 iMEMS® accelerometer measures acceleration with a full-scale range of ±5 g with 1 mg resolution and a temperature range of -40° C to +175° C.
iMEMS Dual-Axis Accelerometer Delivers

Norwood, MA (05/23/2011) - Analog Devices, Inc. (ADI) released for general availability today the ADXL206 high precision, low power, dual-axis iMEMS® accelerometer with signal conditioned analog voltage outputs. The single-chip ADXL206 measures acceleration with a full-scale range of ±5 g and measures both dynamic acceleration such as tilt and static acceleration such as gravity. Offering a guaranteed operating temperature range of -40° C to +175° C and excellent overall stability, the ADXL206 is well suited for geological down hole tools and other extreme high temperature industrial applications.

“Instead of using additional temperature compensation circuitry, innovative design techniques have been used to ensure that high performance is built in,” said Wayne Meyer, marketing and applications manager, MEMS/Sensors Technology Group, Analog Devices. “As a result, there is essentially no quantization error or non-monotonic behavior, and temperature hysteresis is very low, typically less than 2 mg over the entire −40° C to +175° C temperature range. This is another example of ADI's high performance MEMS inertial sensor leadership.”

“As designers put together smart drilling systems that go miles and miles under the earth’s surface, they are challenged to balance power and space requirements against the need for more information,” said Pam Aparo, segment marketing manager for Instrumentation, Analog Devices. “The ADXL206 iMEMS accelerometer is not only an extremely compact solution, but it also lowers power consumption by an order of magnitude from over 10 mA to under 0.5 mA per axis.”

The ADXL206 iMEMS accelerometer has a typical noise floor of 110 μg/√Hz, allowing signals below 1 mg (0.06° of inclination) to be resolved in tilt sensing applications using narrow bandwidths (<60 Hz). Bandwidths of 0.5 Hz to 2.5 kHz can be selected to suit the application. The ADXL206 is available in a 13 mm × 8 mm × 2 mm, 8-lead, SBDIP (side-brazed ceramic dual in-line package) package.

ADXL206 iMEMS accelerometer Key Features

  • -40 °C to +175 °C temperature range
  • 1 mg resolution at 60 Hz
  • Low power: 700 μA at VS = 5 V (typical)
  • High zero g bias repeatability
  • High sensitivity accuracy
  • 3500 g shock survival

Product Sample Availability Full Production Price Each Per 1,000 Packaging
ADXL206 YES YES $789.00 13 mm × 8 mm × 2 mm,
8-lead, SBDIP package

Other high temperature components from Analog Devices include the AD8229, 1.0-nV/√Hz high-temperature instrumentation amplifier, the only low-noise instrumentation amplifier guaranteed to perform at up to 210° C in the most extreme environments.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

iMEMS is a registered trademark of Analog Devices, Inc.

Follow ADI on Twitter at http://www.twitter.com/ADI_News.

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe

Editor's Contact Information:

Howard Wisniowski
781-937-1517

howard.wisniowski@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close