Norwood, MA (06/28/2011) - Analog Devices, Inc. (ADI) released for general availability today the ADIS16210 MEMS iSensor® digital inclinometer system, which provides precise measurements for both pitch and roll angles over a full orientation range of ±180 degrees. The ADIS16210 integrates ADI's iMEMS® multi-axis accelerometer technology and signal processing expertise, adding addressable user registers for application tuning and programming, available over an SPI-compatible serial interface. The precision core sensors are tuned to allow accurate roll/pitch outputs independent of the orientation of the mounted sensor. The ADIS16210 eliminates complex and time consuming user calibration with unit-specific factory calibration, delivering extraordinary 0.1-degree tilt accuracy out of the box. Designed for the most demanding applications, the ADIS16210 is optimized for instruments such as medical scanners that require highly accurate platform stabilization, security and safety monitors, and high-precision platform positioning/steering.
For applications where motion is experienced on every axis and in extreme environments, multi-axis sensing and precision sensor processing is critical. Each ADIS16210 receives extensive calibration and testing to insure a high degree of alignment across each of the three axes and unprecedented tilt measurement accuracy over the full motion range, independent of mounting orientation. This new digital inclinometer system also offers digital accelerometer and temperature sensor measurements together with configuration controls for in-system calibration, sample rate, filtering, alarms, I/O configuration, and power management. The ADIS16210 is available in a 15mm×24mm×15mm module that provides mounting tabs with M2-sized mounting holes and a flexible, edge-terminated connector interface. It has an extended operating temperature range of −40 °C to +125 °C.
| Product | Sample Availability | Full Production | Price each per 1k units |
Packaging |
|---|---|---|---|---|
| ADIS16210 | Now |
Now | $97 | 15 mm × 24 mm × 15 mm module with flexible connector |
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe.
All trademarks are the property of their respective owners.
Howard Wisniowski
781-937-1517
howard.wisniowski@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved