The TMP01 is a temperature sensor that generates a voltage output proportional to absolute temperature, and control signals from one of two outputs when the device is either above or below a specified temperature. Enter high and low temperature trip points and the hysteresis requirements into the input parameters section. The tool will calculate the resulting voltages and corresponding resistor values needed for the circuit diagram shown to the right. The control signal are generated based on the current temperature, setpoint temperatures, and the hysteresis desired.
| Reference Current (Iref) | ___ |
| Voltage Set High | ___ |
| Voltage Set Low | ___ |
| Resistor 1 (R1) | ___ |
| Resistor 2 (R2) | ___ |
| Resistor 3 (R3) | ___ |
| OVER Pin | ___ |
| UNDER Pin | ___ |
If you have any questions, comments, or ideas on how we can improve this tool, please email us!
© 1995 - Analog Devices, Inc. All Rights Reserved